| Function name |
Description |
Applicable Units |
| Free-Run Refreshing |
With this I/O refreshing method, the refresh cycle of the NX bus and the I/O refresh cycles of the NX Units are asynchronous. |
All models |
| Selecting Channel To Use |
This function disables control processing, error detection, and output for unused channels. The conversion time for its own Unit will not be shortened even if errors are disabled. |
All models |
| Input Functions |
Input Type Setting |
This function sets the following input type of sensor input which is connected to the temperature input.
Thermocouple, platinum resistance thermometer, or analog (current: 4 to 20 mA / 0 to 20 mA, voltage: 1 to 5 V / 0 to 5 V / 0 to 10 V) |
All models |
| Temperature Unit Setting (°C/°F) |
This function sets the temperature units for measured values to °C (Celsius) or °F (Fahrenheit). |
All models |
| Decimal Point Position Setting |
This function sets the number of digits displayed after the decimal point for INT type parameters of measured values, set points and alarm values (including alarm upper / lower limits). If the decimal point position for the above-mentioned parameters is fixed in a host device, design changes concerning the decimal point position can be absorbed when replacing a third-party temperature control Unit. |
All models |
| Cold Junction Compensation Enable/Disable Setting |
This function enables or disables cold junction compensation using the cold junction sensor that is mounted on the terminal block when a thermocouple input is used. |
All models |
| Temperature Input Correction |
This function corrects measured values. When there are variations in the sensor or when there is a difference in measured value from other measuring instruments. One-point correction and two-point correction methods are provided. |
All models |
| Input Digital Filter |
This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. |
All models |
| Measuring the Ambient Temperature Around Terminals |
This function measures the temperature around the terminals of the Advanced Temperature Control Unit. |
All models |
| Analog Input Setting |
This function is for analog input and sets the scaling to use the physical analog quantities of current and voltage as inputs for the control application. |
All models |
| Control Processing |
ON/OFF Control |
This control function uses a preset set point to turn off the control output when the temperature reaches the set point during control. |
All models |
| PID Control |
PID control is a combination of proportional (P) control, integral (I) control, and differential (D) control. It is a control function that feeds back the detected value to the set point so that they conform to each other. |
All models |
| Heating/Cooling Control |
This function controls both heating and cooling. |
Heating/cooling control type models |
| Run or Stop Controls |
This function starts and stops temperature control. |
All models |
| Direct/Reverse Operation |
This function specifies direct or reverse operation. |
All models |
| Manual MV (Manual Manipulated Variable) |
This function outputs the specified manipulated variable during PID control. |
All models |
| MV at Error |
This function outputs a fixed manipulated variable when a Sensor Disconnected Error occurs. |
All models |
| MV Limit |
This function adds a limit to the manipulated variable calculated by PID control and outputs it. |
All models |
| Load Rejection MV |
The load rejection means that the connection to the Advanced Temperature Control Unit is interrupted due to a communications error between the CPU Unit and the Communications Coupler Unit host or due to an error on the NX bus.
This function performs a preset output operation if any of the following problems occur.
-The Advanced Temperature Control Unit connected to the CPU Unit cannot receive the output setting values from the CPU Unit due to an NX bus error or CPU watchdog timer error.
-The Slave Terminal cannot receive the output setting values due to a communications error between the Advanced Temperature Control Unit and the Communications Coupler Unit host or due to an error on the NX bus. |
All models |
| Load Short-circuit Protection |
The load short-circuit means that an external device (SSR) connected to the voltage output (for driving SSR) of the Advanced Temperature Control Unit is shortcircuited.
The load short-circuit protection is a function of the Advanced Temperature Control Unit with voltage output (for driving SSR), which protects output circuits of the Advanced Temperature Control Unit when an external device (SSR) connected to the voltage output (for driving SSR) is shortcircuited. |
Models with voltage output (for driving SSR) |
| MV Branch |
The manipulated variables calculated by the slope or offset are output to the branch-destination channel based on the manipulated variables of the branch-source channel. |
Standard control type models |
| Disturbance Suppression (Pre-boost) |
This function suppresses temperature variations by adding a preset manipulated variable before temperature variations occur due to a disturbance. |
Standard control type models |
| Tuning |
AT (Autotuning) |
This is a tuning method that derives the PID constant. This function automatically calculates the PID constant by the limit cycle method according to the characteristics of the control target. |
All models |
| D-AT (Disturbance Autotuning) |
This function automatically calculates disturbance suppression (Pre- boost) function parameters such as FF waiting time, FF operation time, and FF segments 1 to 4 manipulated variables. |
Standard control type models |
| Control Output |
Control Period |
This function sets the period when the ON/OFF time ratio is changed for voltage output (for driving SSR) in time-proportional operation. |
Models with voltage output (for driving SSR) |
| Minimum Output ON/OFF Band |
This function specifies the minimum ON/OFF bands for the heating side control output or the cooling side control output. This function can be used to prevent deterioration of mechanical relays when mechanical relays are used in the actuators connected to the output terminals. |
Models with voltage output (for driving SSR) |
| Output Signal Range Setting |
This function sets the output signal range of the linear current output. You can specify 4 to 20 mA or 0 to 20 mA. |
Models with linear current output |
| Error Detection |
Temperature Alarms |
Function for detecting a deviation or an error in the measured value as an alarm. Alarm operation corresponding to the use can be performed by selecting “Alarm type”. |
All models |
| LBA (Loop Burnout Alarm) |
Function for detecting, as an alarm, the error location in the control loop when there is no change in the measured value while a control deviation equal to or more than the threshold value exists between the set point and the measured value. This function can be used only for temperature input. |
All models |
| Sensor Disconnection Detection |
This function detects disconnections in temperature sensors. It also detects that the measured value of the temperature sensor is outside the input indication range. |
All models |
| Heater Burnout Detection |
This function detects heater burnouts. A heater burnout is detected if the control output is ON and the heater current is equal to or less than the heater burnout detection current. |
Models with CT input |
| SSR Failure Detection |
This function detects SSR failures. An SSR failure is detected if the control output is OFF and the leakage current is equal to or greater than the SSR failure detection current. An SSR failure is a failure that is caused by an SSR short-circuit. |
Models with CT input |
| Predictive maintenance |
Feature Visualization |
This function enables monitoring of features (as feature data) appearing in the control waveform of set point and disturbance responses. |
All models |