FAQ00710 for Level Switches | OMRON Industrial Aut... FAQ00710 for Level Switches | OMRON Industrial Aut...
- ...operation of water drainage, the pump is not turned ON until the level of water reaches the E1. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00710/ 
 faq00716 faq00716
- ...referring to Mounting Weight (2) above. An Insulation Cap is not needed for the long electrode. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00716/ 
 faq00718 faq00718
- ...orrode and have to be regularly replaced. Also, allow at least 1 m of space between Electrodes. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00718/ 
 faq00720 faq00720
- ...vent hole at the top of the pipe. Follow the information above with regard to using Electrodes. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00720/ 
 FAQ00722 for Level Switches | OMRON Industrial Aut... FAQ00722 for Level Switches | OMRON Industrial Aut...
- ...he electrodes open. In the case of a high-sensitivity model, that with 24VAC is also available. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00722/ 
 faq00724 faq00724
- ...for liquids that do not contain a large amount of foreign matter because it is more convenient. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00724/ 
 faq00730 faq00730
- ..., and the terminal arrangement will be reversed, so the wiring will have to be changed as well. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00730/ 
 faq00735 faq00735
- ...ode Holder can be used. F03-14 3P and F03-14 5P can be used only with PS-[]S Electrode Holders. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00735/ 
 faq00736 faq00736
- ... Holders cannot be mounted to it. This means that it will have no protection against vibration. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00736/ 
 FAQ00738 for Level Switches | OMRON Industrial Aut... FAQ00738 for Level Switches | OMRON Industrial Aut...
- ...e is a long distance, but generally they can be treated as the same value without any problems. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...https://www.ia.omron.com/support/faq/answer/33/faq00738/