Primary Contents

Site Search Results

Site Search Product Search IA Global Search
Results 2061 - 2070 of 4388
initial setting level - Glossary index | OMRON Ind...
...tion The appropriate product category Temperature Controllers The setting level used to set the input type, alarm types, and other basic parameters. The Temperature Controller must be stopped...

https://www.ia.omron.com/support/glossary/meaning/3675.html

interrupt response time - Glossary index | OMRON I...
...nition The appropriate product category Programmable Controllers The time required from when an input to an Interrupt Input Unit turns ON until the interrupt task is actually execute...

https://www.ia.omron.com/support/glossary/meaning/3689.html

life expectancy - Glossary index | OMRON Industria...
... service life.The expected service life calculation assumes the following conditions: (1) Rated input voltage, (2) Load rate: 50%, (3) Ambient operating temperature: 40C, (4) Standard mountin...

https://www.ia.omron.com/support/glossary/meaning/37.html

High-speed Counter Unit - Glossary index | OMRON I...
... turn ON an external output when the counted value becomes equal to the set conditions. You can input faster pulse signals to the Unit than a conventional counter to count the number of pulse...

https://www.ia.omron.com/support/glossary/meaning/3772.html

instantaneous safety output - Glossary index | OMR...
... product category Safety Controllers A Safety Output that is turned OFF immediately if a Safety Input, Feedback/Reset Input, or Logical Connection Input becomes invalid....

https://www.ia.omron.com/support/glossary/meaning/3778.html

POSITION CONTROL mode - Glossary index | OMRON Ind...
...e product category Servomotors / Servo Drivers A control mode in which positioning commands are input from a controller and positioning is controlled using the target values in the commands....

https://www.ia.omron.com/support/glossary/meaning/3879.html

forward and reverse drive prohibit - Glossary inde...
...ng beyond the device's travel range by connecting limit inputs. When the Forward Drive Prohibit Input or Reverse Drive Prohibit Input turns OFF, the Servomotor will stop rotating....

https://www.ia.omron.com/support/glossary/meaning/3942.html

function to prevent malfunctions caused by inrush ...
...e product category Networks This function is supported only by Digital I/O Slaves and Bit Slave Input Units. It holds inputs from when the power is turned ON until the Unit stabilizes, i.e., ...

https://www.ia.omron.com/support/glossary/meaning/3982.html

analog data allocation - Glossary index | OMRON In...
...y Networks One of the following six processed values can be selected as the analog data: Analog Input Value, Peak, Bottom, Top, Valley, and Rate of Change. These values can be selected alone ...

https://www.ia.omron.com/support/glossary/meaning/3984.html

comparator - Glossary index | OMRON Industrial Aut...
...appropriate product category Networks This function is supported only by Analog I/O Slaves. The input to the Unit or the calculated data for the Unit can be compared with alarm settings (uppe...

https://www.ia.omron.com/support/glossary/meaning/3985.html

Results 2061 - 2070 of 4388