...duct category Safety Controllers The Safety Application Controller receives signals from safety input devices, which it uses to determine whether a machine should be started or not....
...tegory Programmable Terminals A screen object that displays a list of items that can be used to input a character string or numeric value by selecting one of the items....
...ocal SP Definition The appropriate product category Temperature Controllers A set point that is input with the front-panel keys or communications....
...rol method used to alter the ratio of AC ON and OFF half-waves based on a linear current signal input. This enables accurate control while using an SSR with a zero-cross function....
...roller used to store the output result of a logic operation. A work bit can also be used as the input condition for another logic operation, making more than five AND/OR operations possible....
...duct category Temperature Controllers A function to use the result of logic operation for event input operations, auxiliary outputs, or control outputs. AND or OR operations can be performed ...