...uct category Temperature Controllers The allowable range of error in the indicated value for an input from a sensor. For a thermocouple input, the indication accuracy includes the co...
... output hold time Definition The appropriate product category Power Supplies The time after the input voltage is shut OFF during which the output voltage maintains the constant-voltage precis...
...ing edge of the strobe signal. A strobe signal is required to connect to devices for high-speed input or high-speed response, such as microcomputer boards....
... range Definition The appropriate product category Power Supplies The voltage applied to the AC input terminals. The voltage fluctuation rangeis indicated in parentheses....
...l mode voltage Definition The appropriate product category Digital Panel Indicators Undesirable input voltage superimposed on the measured voltage, such as the thermoelectric force of the con...
... data based on actual measurements. Datasheets give nominal values for the rated current, rated input, rated rotational speed, maximum air flow speed, maximum static pressure, and noise....