...er Description E3Z-LS61 0.5M Compact Photoelectric Sensor with Built-in Amplifier, Square type, Sensing distance: 20 to 200 mm (BGS max setting), NPN open collector, Pre-wired model, 0.5 m E3...
... detection by Muting Sensors A and B. Adjust where Muting Sensors A and B are installed and the sensing direction so that the passage of a person does not interrupt the beams from both Sensor...
...perture angle (directional angle) listed in the catalog specifications is within ±2.5° when the sensing distance for the emitter and receiver is at least 3m. This means that the effective ape...
...ated of Photomicrosensors Used for Industrial Equipment? Answer The following table shows the sensing method and characteristics for modulated and non-modulated light. Non-modulated Modulat...
...s (EE-SX[][][]A,[][][]R) with operation indicators that are lit when light is interrupted (when sensing objects are detected) are available. *1. The Dark-ON⁄Light-ON (selectable) models are n...
... Sensors Lead Contents FAQ No. FAQ01184 Related Contents Primary Contents Question What are the sensing position characteristics of Slot-type Photomicro Sensors? Answer See the following di...
... Sensors with a Slit on the light emitting/receiving window. Reference information: Because the sensing performance of Photomicro Sensors does not have a margin as wide as that for Photoelect...
...the following values as a guide. Slot-type Photomicro Sensors: Approx. 0.025 to 0.05 mm (If the sensing object travels across the shorter side of the light emitting/receiving window.) Reflect...
...ions of the slit for slot-type Photomicro Sensors? Answer It is the same size as the standard sensing object given in the catalog. Example: Standard opaque sensing object measuring...