...to the surface of Ultrasonic Sensors, is the operation affected? Answer Yes, it is. Since the sensing distance becomes shorter than the rated sensing distance, the operation in thi...
...1295 Related Contents Primary Contents Question When a cover is placed on the Ultrasonic Sensor sensing surface, does it affect the sensing? Answer If the cover is within the propa...
... Ultrasonic Displacement Sensor has a long detection distance. Details are provided below. Long sensing distance suits a variety of applications. A setting plug with a temperature compensatio...
...mperature changes. For example, if there is a hot air curtain that causes turbulence within the sensing area, the Ultrasonic Sensors may malfunction. The jetting sound of air nozzles includes...
...o. FAQ01359 Related Contents Primary Contents Question What are the reflective and through-beam sensing methods? Answer Between similar mediums, ultrasonic waves move straight forward, but ...
...nic Sensors Lead Contents FAQ No. FAQ01372 Related Contents Primary Contents Question What is a sensing area of Ultrasonic Sensors? Answer When a standard sensing object enters the...
...ration is possible only when the Sensors are placed at different detection distances, and their sensing ranges do not overlap. E2E Standard Sensors for Detecting Ferrous Metals under Standard...
... Sensors can be used to measure transparent objects. CCDs enable detecting transparent objects. Sensing with a PSD (Not suitable for transparent objects.) A Regular Reflective Sensor that use...
...properly. What is causing this, and what can be done to resolve it? Does the temperature of the sensing object affect the detection ability of E4PA Ultra Sonic Displacement Sensor? When a com...
...properly. What is causing this, and what can be done to resolve it? Does the temperature of the sensing object affect the detection ability of E4PA Ultra Sonic Displacement Sensor? When a com...