...operation The aluminum chips with small density are not detected, and the detection only of the sensing object is enabled by setting the oscillation frequency lower than usually though it is ...
...he TL Series excluding the TL-L100 Series, etc.) If DC/AC magnetic field is 200G or less on the sensing surface of sensor, it is possible to use it. The proximity sensor cannot oscillate and ...
... FAQ01074 Related Contents Primary Contents Question What is "Response time"? Answer When the sensing object moves at high speed and it passes continuously, the response of proximity sensor...
...ors, which reduces the influence of surrounding metal. As shown in Figure 2, the surface of the sensing coil on Unshielded Proximity Sensors is not covered with metal, so flux is also generat...
...Primary Contents Question Can a Capacitive Sensor detect charged objects? Answer Yes, but the sensing distance depends on the charged object and the amount of charge. If the object is charg...
...iameter basically. Please refer to the following so that the idea is different depending on the sensing method. 1. Idea to use the light through the hole Please make the hole of the same size...
... PSD and the dual photodiode are used for the light receiving element and the distance to the sensing object is judged by detecting the reflected light spot position on the light receiving ...
...R, E3S-CR62/67, E32-R21, and E32-R16) or to the E3T. Explanation: The following table gives the sensing distances for the Reflectors listed above. Example: E3Z Reflector Sensing dist...
...ric Sensors, the repeat accuracy is the range of measurement error if the voltage, temperature, sensing distance, sensing object, and angle of the sensing object are the sam...
... light interruption. Diffuse-reflective Sensors may incorrectly detect light incidence, and the sensing distance will decrease.) 2.Photoelectric Sensors cannot be used if the case or lens is ...