...180°. However, install it so that the direction of travel is in the direction of the arrow. The sensing distance will decrease if the magnet section is mounted on a steel plate or other magne...
...nce) of Proximity Sensors may be degraded because of degradation of the internal filling resin, sensing surface resin material, or cable sheath due to ultraviolet light. Stress on Filling Res...
...E Series and TL Series, etc.), please consider that DC/AC magnetic field is 200G or less on the sensing surface of sensor when the sensor is installed. If it is 200G or less, it is possible t...
... Question What is "NO (normal open)"? What is "NC (normal close)"? Answer NO: When there is a sensing object within sensing range, transistor output is ON. NC: When there is not a ...
...tion depending on the capacitance change of this electrode is composed, and the approach of the sensing object is detected by increase of the oscillation amplitude. When the sensing...
...mplifier is changed, the oscillation frequency is changed, and the characteristic change in the sensing distance and the temperature characteristic occurs. Therefore, it is not warrantable th...
...etic field' is caused in a detector coil 2 by generating the eddy current on the surface of the sensing object when the sensing object approaches. Detector coil 1: Only 'Magnetic fie...
...0412 Related Contents Primary Contents Question What is "Response frequency"? Answer When the sensing object moves at high speed and it passes continuously, the response of proximity sensor...
...on occurs in the Proximity Sensor because of the influence of a surrounding metal? Answer The sensing distance is extended, and faulty reset is resulted. Description The sensing di...
...g (2) It remains the state when the sensor detects the object regardless of the presence of the sensing object. (2) It remains the state when the sensor detects the object regardless of the p...