... files? Answer Programmable Controller reporter provides Data collection at Excel loading the input data from CIO or DM area of Programmable Controller pasted at the cells of excel file onl...
... Contents Question Can a single sensor output be connected to multiple Programmable Controllers Input Units in parallel? Answer The conditions for setting up this type of connection are as ...
...ed Contents Primary Contents Question Are there comparison instructions that can be used as the input condition for other instructions in a ladder program? Answer In a CS/CJ-series Programm...
...o CPM1A Programmable Controller Units with a RS-232C cross cable through an adapter, process an input to one CPM1A Unit, and output the result from the other CPM1A Unit? Answer Data in the ...
... Primary Contents Question What is the difference between C200H-ID216 Programmable Controllers’ input Units and C200H-ID218 Programmable Controllers’ input Units? Answer The C200H-...
...ntents FAQ No. FAQ00923 Related Contents Primary Contents Question How do I create a program to input 2-digit BCD data from a digital switch to CIO 0.08 to CIO 0.15 and then move the data to ...
...ntents FAQ No. FAQ00924 Related Contents Primary Contents Question How do I create a program to input 1.5-digit BCD data to CIO 0.00 to 0.05 BCD from a digital switch and move it to a specifi...
...make a program to transfer a 2.5-digit BCD data stored in the DM Area to display it on a static-input digital display (CIO 2.00 to CIO 2.09)? Answer We will assume that CIO 2.10 to CIO 2.15...
...cremental count of N pulse inputs? Answer The following introduces a method to count 32 pulse input bits within a loop program using FOR-NEXT instructions and an index register. (FOR-NEXT i...