Primary Contents

Site Search Results

Site Search Product Search IA Global Search
Results 3251 - 3260 of 4389
faq01874
...nt When the power is turned ON for a Switching Power Supply, a peak current flows to charge the input smoothing capacitor. This is called inrush current. The inrush current value depends on t...

https://www.ia.omron.com/support/faq/answer/22/faq01874/

faq01913
... supplied to the load effectively in the process in which the output voltage starts when the AC input turns ON. When connecting a load (with built-in DC-DC converter) that starts operating fr...

https://www.ia.omron.com/support/faq/answer/22/faq01913/

faq01926
... Primary Contents Question What are switching power supplies? Answer  Switching power supplies input a commercial AC power supply (such as 110 VAC or 220 VAC), uses a high-speed semiconducto...

https://www.ia.omron.com/support/faq/answer/22/faq01926/

faq01967
...es Lead Contents FAQ No. FAQ01967 Related Contents Primary Contents Question Is Power Supplies' input side (primary) isolated from the output side (secondary)? Answer  The primary and second...

https://www.ia.omron.com/support/faq/answer/22/faq01967/

faq01991
...llowing table. Use this information as reference for maintenance and replacement. Conditions: 1.Input voltage: Rated input voltage 2.Load rate: 50% 3.Ambient temperature: 40°C 4.Moun...

https://www.ia.omron.com/support/faq/answer/22/faq01991/

FAQ01127 for Photomicro Sensors | OMRON Industrial...
...nstants R 1 = 220Ω, R L = 10 kΩ Specifications of Connected IC Current I 3 flowing from IC when input voltage is low: 0.1 mA The following is a detailed explanation of the calculation. R 1 = ...

https://www.ia.omron.com/support/faq/answer/24/faq01127/

FAQ01138 for Photomicro Sensors | OMRON Industrial...
...osensor is 0 lx. I L Light current The collector current of a phototransistor under a specified input current condition and at a specified bias voltage. V CE (sat) Collector-emitter saturated...

https://www.ia.omron.com/support/faq/answer/24/faq01138/

FAQ01172 for Photomicro Sensors | OMRON Industrial...
...s Used for Industrial Equipment? Answer  The response time is the delay between when the light input is interrupted and when the control output operates or is released. Generally, the operat...

https://www.ia.omron.com/support/faq/answer/24/faq01172/

faq00024
... during overhead processing, I/O refreshing, and peripheral servicing if C200HS-INT01 Interrupt Input Units are used in CS1 or CS200HX/HG/HE Programmable Controllers? Answer  Yes, if an inte...

https://www.ia.omron.com/support/faq/answer/26/faq00024/

faq00077
...le Controllers using the SYSMAC Support Software? Answer  CPM2C memory contains the following: Input bits: CIO 0 to CIO 9, output bits: CIO 10 to CIO 19, word bits: CIO 20 to CIO 49 and CIO ...

https://www.ia.omron.com/support/faq/answer/26/faq00077/

Results 3251 - 3260 of 4389