faq01475- ...o I program ON/OFF delays? Answer Operation Specifications and Data Trace Results CIO 000000: Input A (CIO 0.00) CIO 000200: Output B (CIO 2.00) *Output B (CIO 2.00) turns ON 3.0 s aft...
https://www.ia.omron.com/support/faq/answer/26/faq01475/
faq01477- ...If the ON and OFF time is 0.5 s or 0.1 s, a Clock Pulse Bit (P_ls and P_0_2s) can be used as an input. The following method can be used to create a flicker program that outputs a pulse-train ...
https://www.ia.omron.com/support/faq/answer/26/faq01477/
faq01479- ...tion How do I program a one-shot output? Answer In a one-shot program, as long as the trigger input stays ON for longer than a certain time (see note), the output bit will be turned ON for ...
https://www.ia.omron.com/support/faq/answer/26/faq01479/
faq01621- ...program an ON delay? Answer Operation Specifications and Data Trace Results CIO 000000: Start input bit (CIO 0.00) CIO 000001: Reset input bit (CIO 0.01) W00000: Work bit to store ...
https://www.ia.omron.com/support/faq/answer/26/faq01621/
faq01823- ...en in Table 1. Instruction Application and characteristics --|↑|-- Can be used only with LD/AND input instructions. DIFU A work bit is required to process the differentiated status. UP A work...
https://www.ia.omron.com/support/faq/answer/26/faq01823/
faq02069- ...in the ladder program in Figure 1, both BINARY ADD instructions and BCD ADD instructions can be input and displayed in decimal form. The data conversion function of CX-Programmer makes this p...
https://www.ia.omron.com/support/faq/answer/26/faq02069/
faq02260- ... specifications. *When one of the pushbutton switches from 1 to 32 is pressed, the two words of input data (4-digit BCD data) will be stored in D100 to D131 as shown in the following example....
https://www.ia.omron.com/support/faq/answer/26/faq02260/
faq02755- ...he KEEP instruction. Figure 1 Basic Functions of the KEEP Instruction In Figure 1, when the set input bit (CIO 0.00) is input as a pulse signal as shown in Figure 2, the output bit (...
https://www.ia.omron.com/support/faq/answer/26/faq02755/
faq02853- ...nd CVM1/CV-series Programmable Controllers CPU Units can accept the differentiation option with input commands. With other models, use DIFU/DIFD, as shown in diagram 2. CJ2 Introducing the Fl...
https://www.ia.omron.com/support/faq/answer/26/faq02853/
faq02892- ...uestion When monitoring a ladder diagram, sometimes the output does not turn ON even though the input condition is ON, or the output turns ON even though the input condition is OFF. ...
https://www.ia.omron.com/support/faq/answer/26/faq02892/