...and Monitoring Relays? These Relays function as alarms for which you can set a threshold value [Input signal*] A voltage, current, temperature (thermocouple or platinum resistance thermometer...
... enables simultaneous monitoring of two physical quantities even in equipment using only analog input devices. You can also see the sensor status Self-diagnostic outputs Self-diagnoses the se...
... enables simultaneous monitoring of two physical quantities even in equipment using only analog input devices. You can also see the sensor status Self-diagnostic outputs Self-diagnoses the se...
...ent power is restored after its start. *1. Refer to “Automatic measurement by arbitrary trigger input” for details on trigger input. Automatic measurement reduce electric shock accid...
...Chronological collection of high-resolution data with fast cycle times NX-HAD High-speed Analog Input Unit Sampling as fast as every 5 μs NX-HTC Advanced Temperature Control Unit Temperature ...
...gurations can also be tested. The TMSimulator also has options for DI and AI Signal Control Box Input Control. This version of TMSimulator works with the following S Series Model robots (HW5....
.../IP and PROFINET Simplified PLC Communication • The VHV5 has one single set of straight forward Input and Output Assemblies used for both EtherNet/IP and PROFINET • The product is offered wit...
...IS NO contacts Normally open contacts (A pair of contacts which are normally open when no relay input is applied.) NC contacts Normally closed contacts (A pair of contacts which are normally ...
... the Power Supply even if the fuse has blown. There is, however, no protection function for the input power lines. Top of page Guideline for Selecting External Fuses and Breakers with Conside...