...ts frequency of automatic measurement allows for understanding the degradation trend, which was so far difficult. K7GE proposes a new way of monitoring insulation. Highly reproducible measure...
...arts feeders, roll presses for secondary batteries, assembly machines for digital products, and so on to detect the presence or absence of workpieces. However, many customers are using fiber ...
...nitoring of motors that frequently change speed, which were difficult to identify abnormalities so far. And simplified condition monitoring device parameter configuration process is contribut...
...t and accurate collection of high‐resolution data in chronological order, the amount of data is so large that the data transfer to databases becomes a bottleneck. [NX5] With approximately fou...
...t having to take a robot out of production. The onscreen display includes a virtual robot stick so users can control the robot just as they would control a physical robot. In addition to the ...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ror displayed in multiple languages [PATENT PENDING] *1 ZP-L’s display supports four languages, so that on-site workers at local factories can understand its configuration. Error displays hav...
...nutes to seconds Result of Learn • Tools arranged in reading order • ROIs (Regions of Interest) so each code can be read uniquely • ROI sized to accommodate the expected positional uncertaint...
... more precise. Machine Operation The NA5-V2 monitors machine status in case of possible trouble so your customers can use your machine with no worry. Quick Troubleshooting + No Need of Mainte...
... using the variable resistor on the dielectric strength testing equipment, or apply the voltage so that it crosses the zero point when it rises or falls. Top of page Maintenance Life Expectan...