...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
...attenuator Not required. Gives means to temporarily block beam. Controls Not required. Controls so located that there is no danger of exposure to accessible emission limit above Class 1 or 2 ...
...nits by making a hole in the bracket and tightening just one nut. • The cable follows the wall, so extra space is not required, and the cable will not get caught on other objects. A Fiber Uni...
... UDP/IP are supported, in addition to FINS messages, FTP file transfers, and mail notification, so that production management can now be organically linked with the production site. The Solut...
...port Services for CX-One OMRON'S CX-One offers many service options in the Internet environment so that engineers and online support is available from anywhere in the world 24 hours a day. On...
...s with very few failures. Massive System Variation We provide a wide variety of RFID components so that users can customize configurations for any installation space or objective, from replac...
... stopped power, standby power, and operating power depending on the power usage conditions so that you can see where energy can be saved. 2) Three-state Energy Classification can be link...
...fe display function The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, t...
...ions with Host Devices Ethernet Connection The compact body also provides an Ethernet connector so that you can transfer read data and images via Ethernet. Smoothly transfer data to PLCs, com...