...LM Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application The load does not turn ON when the Switch is pressed. Why is this? What is the protective structure...
... > Basic Switches Lead Contents FAQ No. FAQ02176 Related Contents Primary Contents Question The load does not turn ON when the Switch is pressed. Why is this? Answer 1. There may be a conta...
...e origin of the equipment to be installed. If a gear linkage is used, do not apply an excessive load to the shaft. Use a tightening torque of 0.49 Nm maximum if Rotary Encoders are to be secu...
...9 10 Next Model Number Description A3PA-90A11-05EG Lighted Pushbutton Switch (Square), Standard load, Square, Single screen, Green, LED (5 VDC), Momentary, SPDT, Case color: Black A3PA-90A11-...
... coil with rated voltage of 100VAC. Is there any problem? What is a failure rate? What types of load are there (resistive loads, inductive loads, lamp and capacitor loads)? A Relay burned out...
...6 7 8 Next Model Number Description A3SA-90A1-05EG Lighted Pushbutton Switch (Square), Standard Load, Square, Single screen, Green, LED (5 VDC), Momentary, SPDT A3SA-90A1-05ER Lighted Pushbut...
... of malfunction. In comparison with the previous method (on the left in the following diagram), load capacity is increased and an exceptionally smooth sliding operation is achieved for long-t...
...Push-In Plus technology are as easy as inserting to an earphone jack. They help reduce the work load and improve wiring quality. Held Firmly in Place Even though less insertion force is requi...
... for multiple heaters? Answer The disconnection detection conditions are listed below. 1. The load current must be 1 A min. 2. The CT detection current must be 30% or higher of the rated ma...