...In Plus terminal blocks are as easy as inserting to an earphone jack. They help reduce the work load and improve wiring quality. Held Firmly in Place Even though less insertion force is requi...
... 3.The switching element in the output circuit turns ON. 4.When the switching element turns ON, load current flows and the lamp turns ON. 5.The input device (switch) is turned OFF. 6.When the...
...le using a carry current of up to 40 A and are used for building into devices, e.g., to turn ON load power supplies. G7Z, G7J, G7X, etc. Work-saving relays ・ Terminal Relays ・ Relay Termina...
...In Plus terminal blocks are as easy as inserting to an earphone jack. They help reduce the work load and improve wiring quality. Held Firmly in Place Even though less insertion force is requi...
...ct a model with a 100 to 240 VAC range or automatic selection of 100 or 200 VAC. 2)What are the load's DC voltage specifications? Example: Select a DC voltage such as 12 VDC or 24 VDC. 3)What...
...rom the Power Supply has stopped. Surge or other overvoltage has been applied externally (e.g., load) to the output side, activating overvoltage protection. Add a varistor and diode to the so...
...r consist of contacts to open and close the electrical circuit for supplying electricity to the load such as electric motor, control coils for allowing contactor to open and close, and an ele...
...he lighting turning ON or OFF. (See note.) Output status Text measurement voltage NPN collector load built-in voltage output The voltage between OUT and is measured using a tester. R: Approx....
...er supplies to control and to input and transformers with sufficient capacities for ratings and load. Not doing so may result in malfunction or failure to operate. Allow only qualified person...
...LM Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application The load does not turn ON when the Switch is pressed. Why is this? The input is not entered into th...