| Site Search | Product Search | IA Global Search |
...sistance with dust-proof and drip-proof construction. • Power supply wiring is not required for input devices. • Connect heavy-load devices (up to 1.5 A). • Power supply wiring is not require...
...ulation function. • Two I/O points can be allocated to any two of the following values: analog input, peak/bottom, top, valley, or rate-of-change. Values without an allocated I/O point can b...
...romotive output as high as that of a thermocouple, thus connecting directly to the thermocouple input terminal of the Temperature Controller is possible. • Four temperature ranges are availab...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...ave been joined by new models with ferrules to help reduce wiring work. • Ideal for the thermal input devices of Temperature Controllers. • Select from a wide variety of Temperature Sensors a...
...amount of heat produced by the Power Supply? What would be the cause and countermeasures for an input breaker tripping or an external fuse blowing? Why does the output indicator light only di...
... as "115% of the current setting value"? Is a specific insertion direction required, and do the input terminals have polarity for the cable of a Zero-phase Current Transformer used with an AG...
...and VDE. • Socket type, same size as MY Power Relays. • Operation indicator provided to confirm input (model numbers with “N” before the suffix). last update: November 6, 2023...
...level can be easily set with a switch. • Mounts to a DIN track or with screws. • Three types of input terminals available: M3 terminals, screwless clamp terminals (detachable), or compact slo...
...ility. (Enlarged sensitivity adjuster and operation selector) • Freely selectable power supply input (24 to 240 VDC, 24 to 240 VAC). (Additional types added to the DC type lineup.) • Mode...
...A-VD Relays. • Prevents malfunction of the G3PA-VD due to residual voltage, leakage current, or input noise. last update: December 19, 2013...
...: December 19, 2013 • Built-in PID control with 2 or 4 control loops or ON/OFF control • Direct input of 7 types of thermocouple or resistance thermometer • 500 ms sampling cycle • RUN/STOP c...
...mation Features Lineup Specifications Dimensions Catalog last update: September 24, 2012 Analog Input Units • Input up to eight analog signals with one Unit. • Functions include line...
... of four inputs in one Unit: resistance thermometer, thermocouple, and DC current/voltage. (The input type is set separately for each input.) • Isolation between input chann...
...l Automation Features Lineup Specifications Dimensions Catalog last update: December 19, 2013 • Input frequencies to 500 kHz. • 32-bit counting range. • Digital variable noise filter provided...
... of four inputs in one Unit: resistance thermometer, thermocouple, and DC current/voltage. (The input type is set separately for each input.) • Isolation between input chann...