| Site Search | Product Search | IA Global Search |
...pler Definition The appropriate product category Solid-state Relays A device that transfers the input signal while isolating the input and output....
... band Definition The appropriate product category Temperature Controllers A restricted range of input changes that do not produce any perceivable change in the output quantity. When this char...
... even if the Counter is reset. The total count value is reset only when a total reset signal is input....
...x | OMRON Industrial Automation UP mode Definition The appropriate product category Counters An input mode in which the Counter starts at 0 and increments the present value by 1 for each coun...
...| OMRON Industrial Automation DOWN mode Definition The appropriate product category Counters An input mode in which the Counter starts at the set value and decrements the present value by 1 f...
...ters A mode in which an output is repeatedly turned ON and OFF for the set times when the start input turns ON....
...lay with a type of stepping operation, where the contacts alternate between ON and OFF for each input pulse....
...priate product category Timers A control device that outputs a signal at a preset time after an input signal is received....
...e appropriate product category Temperature Controllers An active control to compare temperature input signals and provide output regulation to a heating and or cooling process....
...on Programmable Terminals Definition The appropriate product category Programmable Terminals An input device with a touch panel enabling operation on screens created by the user. If you use a...
.... Three actions are output (open, close, and do not open or close) and the amount of opening is input as feedback using a resistance value....
...ipulated variable. Manual operation is used to output the manipulated variable that is manually input from front-panel keys. Auto/manual switching is used to switch between these....
...unt that serves as the target for feedback control. The abbreviation is SP. If the set point is input with key operations or communications, it’s called the local SP. If the set point is...
...imum or minimum measured value up to the point where the power supply is turned ON or the RESET input is turned ON....
...The appropriate product category Counters The ratio between the ON time and OFF time of a count input signal. (The maximum counting speed of a counter is specified at an ON/OFF ratio of 1:1.)...
... Definition The appropriate product category Temperature Controllers The MV to output when a PV input error, RSP input error, or other error occurs....
...on The appropriate product category Timers Operation in which the output turns ON as soon as an input is received and turns OFF after the set time....
...munications software, a modem, or a host computer. An echoback is used to confirm if characters input from a keyboard are transmitted correctly. Echobacks are not performed or are replaced wi...
...category Counters A function that forces the displayed frequency to return to zero when a pulse input is not received within a specified period of time during frequency measurement processing...
...ne made with many straight lines to compensate for the non-linear (curved) characteristic of an input....