Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 4681 - 4700 of 41292
prescaling function - Glossary index | OMRON Indus...

...e appropriate product category Counters A function of a tachometer in which the frequency of an input pulse is converted to the desired unit, such as revolutions per minute, revolutions per s...

https://www.ia.omron.com/support/glossary/meaning/4208.html

hold function - Glossary index | OMRON Industrial ...

...riate product category Digital Panel Indicators A function for stopping measurement when a HOLD input turns ON and holding the display value from immediately before the HOLD input tu...

https://www.ia.omron.com/support/glossary/meaning/4228.html

Digital Panel Indicators - Glossary index | OMRON ...

...s, currents, other analog signals, and pulse signals. Digital Panel Indicators can also compare input values to set values, transfer data, and perform other functions....

https://www.ia.omron.com/support/glossary/meaning/4365.html

current - Glossary index | OMRON Industrial Automa...

... Definition The appropriate product category Power Supplies The current value flowing to the AC input terminals. This value is the stable current and will fluctuate depending on the load....

https://www.ia.omron.com/support/glossary/meaning/4398.html

rated voltage - Glossary index | OMRON Industrial ...

...The appropriate product category Solid-state Relays A voltage that serves as a standard for the input signal....

https://www.ia.omron.com/support/glossary/meaning/4449.html

operating time - Glossary index | OMRON Industrial...

...tegory Timers The time required for time-limit contacts to complete operation for the specified input....

https://www.ia.omron.com/support/glossary/meaning/4453.html

AC relay - Glossary index | OMRON Industrial Autom...

... The appropriate product category General Purpose Relays A Relay designed to operate with an AC input....

https://www.ia.omron.com/support/glossary/meaning/47.html

frequency - Glossary index | OMRON Industrial Auto...

...on The appropriate product category Power Supplies The frequency of a voltage applied to the AC input terminals....

https://www.ia.omron.com/support/glossary/meaning/57.html

tachometer - Glossary index | OMRON Industrial Aut...

...opriate product category Counters A function that measures rotations or speeds based on a pulse input. The measured value can be converted to any desired unit using a prescaling function....

https://www.ia.omron.com/support/glossary/meaning/733.html

linearity - Glossary index | OMRON Industrial Auto...

...gory Pressure Sensors / Flow Sensors The degree of deviation from a linear relationship between input and output signals. (The degree of linearity is generally indicated as a percentage of th...

https://www.ia.omron.com/support/glossary/meaning/88.html

DC Relay - Glossary index | OMRON Industrial Autom...

...n The appropriate product category General Purpose Relays A Relay designed to operate with a DC input....

https://www.ia.omron.com/support/glossary/meaning/89.html

dead band - Glossary index | OMRON Industrial Auto...

... band Definition The appropriate product category Temperature Controllers A restricted range of input changes that do not produce any perceivable change in the output quantity. When this char...

https://www.ia.omron.com/support/glossary/meaning/94.html

pulse measurement method - Glossary index | OMRON ...

...asurement method Definition The appropriate product category Counters A method for measuring an input pulse with a tachometer. The pulse measurement method in which pulses are counted over a ...

https://www.ia.omron.com/support/glossary/meaning/944.html

explanation_of_terms.html

... not provided with a control output. Addition (Up/Incrementing) Counter A Counter having an add input and thus capable of counting in an ascending order. Subtraction (Down/Decrementing) Count...

https://www.ia.omron.com/support/guide/11/explanation_of_terms.html

explanation_of_terms.html

...e, and power supply voltage) can be repeatedly detected. Response time The delay from the light input turning ON/OFF until the control output operation or release operation. The following equ...

https://www.ia.omron.com/support/guide/24/explanation_of_terms.html

explanation_of_terms.html

...utside of the PLC and the I/O response time are also longer, making it impossible to receive an input signal that is shorter than the cycle time. When the cycle time is short, I/O response ti...

https://www.ia.omron.com/support/guide/26/explanation_of_terms.html

explanation_of_terms.html

...nsors. Detection is not possible in this area. Response time The delay time from when the light input turns ON or OFF until the control output operates or resets. In general for Photoelectric...

https://www.ia.omron.com/support/guide/43/explanation_of_terms.html

explanation_of_terms.html

... the drive mechanism in an external Servo Drive or the sensing mechanism in an external Encoder Input Slave Unit. Axes Group A functional unit that groups together axes within the Motion Cont...

https://www.ia.omron.com/support/guide/454/explanation_of_terms.html

explanation_of_terms.html

... the zero point, the phases must be the same. Phase difference may result in malfunctions. (The input signal and output value will not match.) Duty Setting As shown in the following graph, ch...

https://www.ia.omron.com/support/guide/54/explanation_of_terms.html

further_information.html

...en an Average-value-rectification Converter and an Effective-value-calculation Converter if the input is a sine wave. Neither type is better than the other. There is a general misunderstandin...

https://www.ia.omron.com/support/guide/63/further_information.html

Results 4681 - 4700 of 41292

Select Country in