| Site Search | Product Search | IA Global Search |
... service life.The expected service life calculation assumes the following conditions: (1) Rated input voltage, (2) Load rate: 50%, (3) Ambient operating temperature: 40C, (4) Standard mountin...
... turn ON an external output when the counted value becomes equal to the set conditions. You can input faster pulse signals to the Unit than a conventional counter to count the number of pulse...
... product category Safety Controllers A Safety Output that is turned OFF immediately if a Safety Input, Feedback/Reset Input, or Logical Connection Input becomes invalid....
...e product category Servomotors / Servo Drivers A control mode in which positioning commands are input from a controller and positioning is controlled using the target values in the commands....
...ng beyond the device's travel range by connecting limit inputs. When the Forward Drive Prohibit Input or Reverse Drive Prohibit Input turns OFF, the Servomotor will stop rotating....
...e product category Networks This function is supported only by Digital I/O Slaves and Bit Slave Input Units. It holds inputs from when the power is turned ON until the Unit stabilizes, i.e., ...
...y Networks One of the following six processed values can be selected as the analog data: Analog Input Value, Peak, Bottom, Top, Valley, and Rate of Change. These values can be selected alone ...
...appropriate product category Networks This function is supported only by Analog I/O Slaves. The input to the Unit or the calculated data for the Unit can be compared with alarm settings (uppe...
...on is supported only by Analog I/O Slaves. The top/valley hold function holds the top or valley input value to an Analog Input Unit. The Top/Valley Detection Timing Flag can be used ...
...alog I/O Slaves. The peak/bottom hold function holds the maximum (peak) or the minimum (bottom) input value to an Analog Input Unit. The maximum (peak) or minimum (bottom) value can ...
...ed only by Analog I/O Slaves. The user adjustment function can be used to compensate offsets in input (or output) values that occur due to the features of or connection method used for ...
...is supported only by Analog I/O Slaves. The cumulative counter calculates the integral time for input (or output) analog values and reads the cumulative value. Monitor values can be set in Un...
... This function is supported only by Digital I/O Slaves and Bit Slaves. The number of times each input contact or output contact is turned ON can be counted at a sampling frequency of 50 Hz ma...
...y by Digital I/O Slaves and Bit Slaves. The Slave Unit can quickly measure the ON/OFF timing of input and output contacts without relying on the ladder program. Contact types (IN - OUT, OUT -...
...y Analog I/O Slaves. You can find the rate of change during the set data sampling cycle for the input value to an Analog Input Unit. The settings are made by using the CX-Integrator....
...time Definition The appropriate product category Power Supplies The time required from when the input voltage is turned ON until the output voltage reaches 90% of the rated output voltage....
...pler Definition The appropriate product category Solid-state Relays A device that transfers the input signal while isolating the input and output....
... function is supported only by Analog I/O Slaves. The Disconnected Line Detection Flag for each input can be used in the Master Unit to check whether the analog input lines (for volt...
...ts a measured present value as the set value. Teaching can be used instead of operating keys to input the set value....
... is reached. The status of the batch output is retained until the batch counter reset signal is input....