| Site Search | Product Search | IA Global Search |
...er a set period of time after the contacts of the timer are switched when the timer receives an input....
... product category Counters A reset that results from applying the specified signal to the reset input signal terminal....
...opriate product category Counters A counter that increments the count value each time the count input is received....
...opriate product category Counters A counter that decrements the count value each time the count input is received....
...e Definition The appropriate product category Temperature Controllers The shortest time that an input signal must be ON in order to detect it....
...ition The appropriate product category Power Supplies The output power divided by the effective input power. The higher the efficiency (a percentage), the lower the internal loss in the Power...
...ital Panel Indicators Noise voltage that is caused by external induction and appears at the two input terminals. It has the same amplitude and phase at both input terminals. The comm...
...of signals are fast. This allows a long cable distance. They can be connected to open-collector input devices (NPN or PNP)....
...uct category Temperature Controllers The allowable range of error in the indicated value for an input from a sensor. For a thermocouple input, the indication accuracy includes the co...
... output hold time Definition The appropriate product category Power Supplies The time after the input voltage is shut OFF during which the output voltage maintains the constant-voltage precis...
...used by the resistance of the compensating leads and other components when using a thermocouple input....
...ry General Purpose Relays A Relay that turns multiple contacts ON and OFF in order each time an input pulse is received....
...ing edge of the strobe signal. A strobe signal is required to connect to devices for high-speed input or high-speed response, such as microcomputer boards....
...tegory Timers The time required for time-limit contacts to complete operation for the specified input....
... range Definition The appropriate product category Power Supplies The voltage applied to the AC input terminals. The voltage fluctuation rangeis indicated in parentheses....
...l mode voltage Definition The appropriate product category Digital Panel Indicators Undesirable input voltage superimposed on the measured voltage, such as the thermoelectric force of the con...
... data based on actual measurements. Datasheets give nominal values for the rated current, rated input, rated rotational speed, maximum air flow speed, maximum static pressure, and noise....
...tortion Definition The appropriate product category Networks The difference or ratio between an input and output pulse widths....
...and the set value. The proportional band is given in industrial units or as a percentage of the input range. If the proportional band is increased, the change in the manipulated variable will...
... Definition The appropriate product category Networks The number of TTL gates to which a single input terminal corresponds....