| Site Search | Product Search | IA Global Search |
...irection. (Maintain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. •When two or more ...
https://www.omron.com.tw/products/family/3669/dimension.html
...e theme on both the piping side and the sensor mounting side. Because the sensor is designed so that the measurement area is in the center of the piping, correct measurement may not be ...
...LT01C-V4 CXONE-LT01C-V4-UP CX-One Lite Ver.4.0 includes CX-Programmer Ver.9.0 (Micro PLC only), so upward compatible. Model Body Color Dimen sions Wire connection Mounting Dimensions Charact ...
https://www.fa.omron.com.cn/upload/alternative/PRDN-2010057E.pdf
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.fa.omron.co.jp/data_pdf/closed/cat/timer_replace_tg_e_1_1_csm1062339.pdf
...ation devices used on ships must conform to classification standards of individual countries if so requested by the owner. Regulation (EC) No. 391/2009 of the European Parliament and of the C...
...t work properly. Performance Cookies These cookies allow us to count visits and traffic sources so that we can measure and improve the performance of our website. They help us to know which p...
...ed in JIS K 2241:2000; Temperature: 35 °C max.) *2. The optical fiber is 2 m long on each side, so the sensing distance is 4,000 mm. Note: 1. The following mode names and response times apply...
...NX-SL3300 1024點 2048KB 128 自由運轉方式 Ver. 1.1 NX-SL3500 註. 關於安全CPU模組NX-SL5[][][]型,請參閱NX-CSG/SL5/SI/SO產品資料表(http://www.omron.com.tw)。 附屬品 無附屬品。 自動化軟體 Sysma...
...類 額定/性能 外觀尺寸 型錄/操作手冊/CAD/軟體 更新日期 2025年7月18日 認證標準 ●NX系列安全控制模組 NX-SL3/SI/SO型 認證機關 規格 TÜV Rheinland * •EN ISO 13849-1 •EN ISO 13849-2 •IEC 61508 part...
https://www.omron.com.tw/products/family/3243/specification.html
...3. Remove the tape and measure the temperature. Set the emissivity on the Infrared Thermosensor so that the temperature measures the same as when the tape was on the object. Data Collecti...
...關 連接數 I/O更新 方式 安全輸入模組 4 點 2 點 Sink輸入 (PNP) DC 24V 1 自由運轉 方式 Ver.1.1 NX-SIH400 註.詳情請參考NX-SI/SO安全控制模組 選購品 感測器安裝金具 外觀 型號 E39-L104 防止相互干擾濾...
...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...
...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...
...mA max. Note: 1. Alarm signal output is not equipped with an internal current limiting circuit, so be sure that the current flowing to the alarm signal output terminals does not exceed 50 mA....
https://www.omron.com.tw/products/family/3780/specification.html
...s should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron.com.tw/products/family/3809/dimension.html
...s should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron.com.tw/products/family/3810/dimension.html
...ld be 1 to 5 mm. Note: 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron.com.tw/products/family/3899/dimension.html
...模組使用手冊」(Man.No.:SGFM-710)。 種類 型號 OMRON製 單光束安全感測器 E3ZS OMRON製 非接觸式安全門開關 D40A-2, D40A 安全輸出模組NX-SO 種類 外觀 規格 模組版本 型號 安全輸出 點數 內部I/O 共通...
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron.com.tw/products/family/3937/dimension.html