| Site Search | Product Search | IA Global Search |
...s, Ltd. --- * There is a risk of quality problems when using cables assembled by typical users, so we recommend purchasing cables with preattached connectors or having a qualified technici...
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.ia.omron.com/products/family/1498/specification.html
...en the Spacer is not used. * With the E3S-2E4 (41), use the Spacer as shown in the figure above so that the supporter and Mounting Bracket will not be struck when the optical axis is adjus...
https://www.ia.omron.com/products/family/1568/dimension.html
...termined for the current and power that can be provided to the mounted Units. Design the system so that the total current consumption for all the mounted Units does not exceed the maximum tot...
https://www.ia.omron.com/products/family/1639/specification.html
...M Area.) Note 1. Errors and fluctuations will increase when the input signal pulse rate is low, so specify a longer time unit. Note 2. The instantaneous value is only refreshed at intervals o...
https://www.ia.omron.com/products/family/1671/specification.html
...ies, Ltd. - * There is a risk of quality problems when using cables assembled by typical users, so we recommend purchasing cables with preattached connectors or having a qualified technicia...
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
... time. *2. The Data Collection Patterns use the data collected by the Basic Collection Pattern, so the data will be collected at the Basic Collection Pattern’s interval even if the Dat...
https://www.ia.omron.com/products/family/1732/specification.html
... hot start is performed when the power supply has been OFF for only a short time, so in those cases the inrush current values may be higher (as much as two times higher) than th...
https://www.ia.omron.com/products/family/1778/specification.html
...eries Controllers only. *2. Drop-line connections are not supported with a baud rate of 4 Mbps, so Slaves with prewired cables (Bit Slaves) cannot be used. *3. Round cable, Flat Cable,...
https://www.ia.omron.com/products/family/1779/specification.html
...ns manual startup mode I/O Communications Manual Startup Mode can be set from the CX-Integrater so that remote I/O communications are not started when the power is turned ON.Remote I/O commun...
https://www.ia.omron.com/products/family/1781/specification.html
...model most suited to the application. *3. Set the distance between the Sensor and the Reflector so that it is at least the value in parentheses. Accessories Sensor I/O Connectors (Sockets on ...
... power ON time. 2. Do not use the Timer with a repeat period of less than 3 s. Doing so may result in abnormal heating or burning. Refer to Safety Precautions (H3C...
https://www.ia.omron.com/products/family/1891/specification.html
...d if a hot start is performed when the power supply has been OFF for only a short time, so in those cases the inrush current values may be higher (as much as two times higher) than th...
https://www.ia.omron.com/products/family/1916/specification.html
...registers for storing PLC memory addresses for indirect addressing. (Index Registers can be set so that they are unique in each task or so that they are shared by all tasks.) Cyclic ...
https://www.ia.omron.com/products/family/2045/specification.html
...llows for repetition of a given operation, start/end of operation data via external inputs, and so on. Accordingly, the PCU can perform various operation sequences without affecting the ladde...
https://www.ia.omron.com/products/family/2051/specification.html
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
.... On the model Z-15GQ8-B, the M3 hole with a depth of 10 mm is a through hole. Take precautions so that no water or screw lock agent penetrates into the hole. Panel Mount Roll...
... not use both the M12 mounting screw and the mounting holes in the case at the same time. Doing so will cause stress to be applied to the Switch, possibly damaging the case or cove...