| Site Search | Product Search | IA Global Search |
... directly or indirectly. Do not use it for such purposes. Do not disassemble the product. Doing so may cause electric shock due to the high voltage portion. Burn also may result due to high t...
https://www.omron.com.au/data_pdf/mnu/zw-5000_inst-9308560-9e.pdf
...ve cap Important Important ・If attaching the protection cap, be careful with the cable bear and so on when routing the cable via it. The protection cap could be trapped by the cable bear. ・Wh...
https://www.omron.com.au/data_pdf/mnu/zw-xf50__r_inst-9308786-5b.pdf
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. You can pickup the product safely with Safely-Limited Speed function...
https://www.omron.com.tw/data_pdf/cat/1s_series_i858-e1-01.pdf
...ing these sensors together with the e-jig allows you to easily upgrade your existing facilities so that you can replace their sensors in just 10 seconds.*1 1. Dismount the M18 proximity senso...
https://www.omron.com.tw/data_pdf/cat/e2e_d121-e1_3_5_csm1067251.pdf
...sity of the light received by the sensor from highly-reflective glossy packaging is too strong, so there is not enough difference in incident levels to perform color mark detection (i.e. satu...
https://www.omron.com.tw/data_pdf/cat/e3s-dc_e3nx-ca_y216-e1_1_9_csm1052116.pdf
...ection. (Main- tain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the water- proof packing onto the Controller. •When two or mor...
https://www.omron.com.tw/data_pdf/cat/e5_d-800_h226-e1_1_5_csm1057810.pdf
...ection. (Main- tain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the water- proof packing onto the Controller. •When two or mor...
https://www.omron.com.tw/data_pdf/cat/e5_d_e5_d-h_h223-e1_2_2_csm1057808.pdf
...nt malfunction or adverse affects on the performance or functionality of the product. Not doing so may occasionally result in faulty operation. 1. This product is specifically designed for in...
https://www.omron.com.tw/data_pdf/cat/e5_n_e5_nh_e5_n-ht_cn_e_3_5_csm1373.pdf
...uction in processing quality. •The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. You can use a rise in hydraulic oil temperatu...
https://www.omron.com.tw/data_pdf/cat/e8fc_e8pc_e472-e1_4_3_csm1065029.pdf
... more components Only 2 Sensor The camera and lighting have been integrated into a single unit, so only one camera mounting bracket is required. The Sensor co mes with a multi-directional mou...
https://www.omron.com.tw/data_pdf/cat/fq2_q193-e1_15_2_csm1006918.pdf
... and detachment prevention of relays are achieved by locking and unlocking of stopper. Designed so that wires are hard come out even if release levers are touched unintentionally. Visibility ...
https://www.omron.com.tw/data_pdf/cat/g2rv-st_g3rv-st_j265-e1_2_10_csm1121815.pdf
... prevent malfunction. Transport Do not transport the G3PE under the following conditions. Doing so may result in damage, malfunction, or deterioration of performance characteristics. •Conditi...
https://www.omron.com.tw/data_pdf/cat/g3pe_j174-e1_2_1_csm2137.pdf
...lotted in graphs to provide this data. Use this data only as a guide. Relays are mass-produced, so allowances must be made for a certain amount of variation in measurement data. 2. The data s...
https://www.omron.com.tw/data_pdf/cat/g6b-4__nd_g3s4_ds_e_5_1_csm1057979.pdf
... is connected to two or more Timers, the input terminals of those Timers must be wired properly so that they will not differ in phase, otherwise the terminals will be short-circuited to one a...
https://www.omron.com.tw/data_pdf/cat/h3cr_l084-e1_3_6_csm1013792.pdf
...t •The transistor output of the H7CC is isolated from the internal circuitry by a photocoupler, so the transistor output can be used as both NPN and PNP output. •The diode connected to the co...
https://www.omron.com.tw/data_pdf/cat/h7cc_m094-e1_2_10_csm1106903.pdf
...sier to understand, and the present value display can be switched between red, green and orange so that output status can be seen from a distance. Note: The H5CX-A11 and H5CX-L8 Timers have o...
https://www.omron.com.tw/data_pdf/cat/h7cc_m095-e1_3_1_csm1106892.pdf
...open-collector output of the K7L-U/UB is isolated from the internal circuits by a photocoupler, so you can use either an NPN open- collector output or a PNP (equivalent) output. K7L-UD/UDB K7...
https://www.omron.com.tw/data_pdf/cat/k7l_n211-e1_6_7_csm1050158.pdf
...terminals. •Connect a branch circuit breaker between the voltage input terminals and the wiring so that the power supply can be turned OFF immediately. •For safety, always work with the power...
https://www.omron.com.tw/data_pdf/cat/km-n2_km-n3_n213-e1_3_13_csm1050147.pdf
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron.com.tw/data_pdf/cat/nx-tc_nx-htc_h229-e1_2_2_csm1061207.pdf
... When you use any ferrules other than those in the above table, crimp them to the twisted wires so that the following processed dimensions are achieved. Using Twisted Wires/Solid Wires If you...
https://www.omron.com.tw/data_pdf/cat/nx-ts_hb_ds_e_4_2_csm1057423.pdf