| Site Search | Product Search | IA Global Search |
....g., Retroreflective, Diffuse-reflective, Convergent-reflective, or Distance-settable Sensors). E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...
...Sensors with built-in amplifier, the sensing distance is 3 m whether E39-R1 or E39-R1K is used. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...
...ing Through-beam Sensors are recommended for detecting sensing objects like those listed above. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...
...apply for use in combination with the E3X-DA-S Amplifier Unit (general-purpose, standard mode). E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...
...the E32-C31), the holes that the fibers are inserted into are set for the receiver and emitter. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...
...nt to the F150 Vision Sensor. These are the F150, F160, F180, F210, F250, F270, F400, and F500. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How can a stored im...
...e extension. Therefore, it is recommended that the F160-KP should be used with standard length. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How can a stored im...
...tance decreases. Thus, use the K7L with maximum sensitivity to detect almost all of impurities. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...uding metal powders, it may be detected. Confirm the above by evaluating with actual equipment. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...peration. Connect one Sensing Band to each Terminal Block. Note: 2. Not applicable to K7L-AT50D E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...r to earthquakes are probably being detected in that area, so change the installation location. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...on of the output waveform is the resolution of the measurement device, such as an oscilloscope. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...1° max. The intermittent and continuous outputs are output from the same open-collector output. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How much inclinatio...
...lected waves are non-uniform. However, it is less affected by the gradient of a sensing object. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...or), noise filter (e.g., ferrite core or insulated transformer), or varistor in the power line. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...easure: Place the Sensors apart from one another so that they do not interfere with each other. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...off a surrounding object, it may affect the detection characteristics of the Ultrasonic Sensor. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...equency, and the types of oscillators are determined depending on the required operating range. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...an the rated sensing distance, the operation in this kind of environment cannot be recommended. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...
...cable for the E4C-TS50S.) For the E4R, use an 11/0.16-dia. parallel 1-conductor shielded cable. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the highest...