| Site Search | Product Search | IA Global Search |
...rent frequencies are available to stagger the oscillating frequencies of the Proximity Sensors. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...s? Answer Refer to the following figures, which apply to Sensor A being affected by Sensor B. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...Question Please teach the principle of operation of Standard cylinder type Proximity Sensor the E2E Series. Answer The circuit composition and the principle of operation are as follows. 1. ...
... moving direction of sensing object is parallel to the sensing surface of the proximity sensor. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...ove Proximity Sensors cannot be used in a sereis connection. If needed, connect through relays. E2E-X[]Y For the above Proximity Sensors, the voltage VL that can be applied to the load when O...
... electronic components, resin, and cables). Use Sensors within the specified temperature range. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...r Please note that there is a possibility of breaking down when wiring by mistake as follows; E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...hrobs Please put the bleeder resistance in parallel with the load. (Refer to the figure below.) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...r to Figure 2.) Figure 1: Basic Construction of a Reed Switch Figure 2: GLS Operating Principle E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...ted on a steel plate or other magnetic object. Check the sensing distance before operating GLS. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...encies coming close together, so mount the Sensors at distances of at least the catalog values. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...power supply line ④ Noise from earth conductor ⑤ Radio noise Noise from wireless applications ⑥ E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...rcuited with power supplies in some factors. (3) The following is output circuit diagram of the E2E as typical. E2E Standard Sensors for Detecting Ferrous Metals under Standard Condi...
... with a hood or installed in a resin box to prevent exposure to ultraviolet light and freezing. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...of the magnetic field is not received. (3) For high frequency oscillation proximity sensor (the E2E Series and TL Series, etc.), please consider that DC/AC magnetic field is 200G or less on t...
...in sensing range, transistor output is ON. NO/NC selectable: NO/NC selectable is by switch etc. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
... potential grows by the relative permittivity large and it is easy for the sensor to detect it. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...ensor? Answer Yes, it provides as follows in each type of the sensor. Built-in amplifier (the E2E Series, the TL Series) The following occur. Voltage descent by resistance component of cabl...
...t magnetic field' When there is no detection object: Difference between coil 1 and coil 2= none E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...
...ct is repeatedly brought into proximity. See the accompanying diagram for the measuring method. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...