| IAグローバル検索 |
...iatura del riscaldatore, assumendo la corrente di minore amperaggio come valore di bruciatura. (Se tutti i riscaldatori usano corrente con lo stesso amperaggio, usare il valore applicabile ad...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/e5cn_e5cn-h(eventinput)_inst-3089286-5b.pdf
...VDC21tTA 「一① →《reSlgbveloed) 一毘6m`③ ●4 ◆5 一AB8 留③◎⑤ ⑤⑦◎⑥⑩ ThettnOOOuPte Donorv5e OOnotU6e Oonet"se P`at巾om了6gs恰nc8肋8mome86「 ●E5CSZ・RST口1-Q1了口(AIarmoutpvttype} 一 Ywefsupρ|y .1...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/e5csz_inst-1649996-4c_discon.pdf
...礽 ches + en礽 foncées pendant au moins 1 secon礽 de drücken (kürzer als 1 Sekunde) minde礽 stens 3 Se礽 kunden gedrückt halten minde礽 stens 1 Se礽 kunde gedrückt halten und minde礽...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/e5gn(eventinput)_inst-1178067-3a.pdf
...E]key. 3) is indicated. Pus h the[MODE]key. 4) Hysteresis width of OUT1is indicated. Change the se tting by[UP]or[DOWN]key. 5) Fix the setting by[MODE]key. 6) is indicated. Pus h th...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/e8y-a5c-f____inst-0696699-8a.pdf
...orUse (1)SensitivitySe【1ing ・Thcfac【oryscttingi3scttos㎝slngscmiconductorsilLcan ≠ぶnd血mmyw血S(㎜」皿㎜seロsjtiVirySCtring), 50be3ure10cha血gclhCSettingaccordi血gto:hcobjectfbr d創cction....
https://www.fa.omron.com.cn/data_pdf/closed/mnu/f3m-s6___-s8___inst-0699640-4d_en.pdf
...sc]【ibesthefeaturesof gene『alfeaturesof theES100X,namesofpa蝋s,ξmdtypi一 theES100X calfUnctions. ●Se廿ingupthe Chapter2Prepa】rations Thischapterdescribestheoperations E釦00X thatyoumUStC姫...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h070-e1-02_es100x.pdf
...ide the alarm range. For example, if the alarm mode is set to Lower-limit Alarm without Standby Se- quence, and the ambient temperature is lower than the alarm set value (i.e., within the ala...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h076-e1-02_e5ze.pdf
...otectmode or to return to the level 0 mode fromthe protectmode, press the A/M key and key for 1 se- condminimumsimultaneously. •To set the controller to themanual mode, press the A/M key for ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h083-e1-03_e5ak.pdf
...otectmode or to return to the level 0 mode fromthe protectmode, press the A/M key and key for 1 se- condminimumsimultaneously. •To set the controller to themanual mode, press the A/M key for ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h085-e1-03_e5ek.pdf
...HAPTER 1 INTRODUCTION E5AK 1--6 Add on the input unit (E53-CKB) when using event input. You can se- lect from the following six event inputs: Run/Reset, Remote/Local, Auto/Manual, Hold/Hold C...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h088-e1-02_e5ak.pdf
...HAPTER 1 INTRODUCTION E5EK 1--6 Add on the input unit (E53-CKB) when using event input. You can se- lect from the following five event inputs: Run/Reset, Auto/Manual, Hold/Hold Cancel, Advanc...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h089-e1-02_e5ek-t.pdf
...otectmode or to return to the level 0 mode fromthe protectmode, press the A/M key and key for 1 se- condminimumsimultaneously. •To set the controller to themanual mode, press the A/M key for ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h099-e1-02_e5ek-drt.pdf
...larm values Start operation Start program execution Control stops. Control period (heat) (unit: se- conds) Alarm 1 type Control starts. Process value/ set point Alarm value 1 Adjustment level...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h112-02a_e5an.pdf
...ntrol point being auto-tuned. 3. When the E5ZE is turned ON, the memory bank numbers previously se- lected through communications will be effective. Setting Data Range @ R % s Terminator * Al...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h114-e1-01_e5ze-8-v2.pdf
...hange 1 0 0 001 Reset Error 1 0 1 1010 0 0 0 0 00 Alarm 1 Latch Cancel 1 1 0 010 (See note 2.) (Se e not e 4.) Alarm 2 Latch Cancel 1 1 0 011 Alarm 3 Latch Cancel 1 1 0 100 All Alarm Latch Ca...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h143-e1-01_ej1g.pdf
...nd op- erating panel, attach a water- proof packing (Model Y92S-29) in the space and be sure to se- cure it by tightening screws of the flush-mounting adapter (Model Y92F-30). Upper limit Low...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h7cx-r_inst-1617581-6a_en.pdf
...key to selectthedesiト edinputmode. ⑥Selectionof outputmode RI c 、附トリ NIド Depress the \」±」key to se一e ctthedesi卜 edoutputmode. 2.PresettingofNumericValue .To presetnumericvalues,fir...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/h8ca-s_inst-0667338-9b_en.pdf
...ock Input power supply can be connected to any terminal on the terminal block because the phase se- quence of input power supply is irrelevant to the phase sequence (R/L1, S/L2, and R/L3). D ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/i528-e1-05_3g3jv.pdf
...th their superior performance and fast response, plus a wider selection of models, the OMNUC W -se- ries AC Servomotors and Servo Drivers inherit the features of and surpass the previous OMNU...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/i531-e1-09_r88m-w_r88d-w.pdf
...ct2 purposes. Table 2.16 Control Circuit Terminals Type No. Signal2 Name Function Signal2 Level Se- quence2 input2 signals S1 Forward2 run/stop2 command Forward2 run2 when2 ON;2 stopped2 when...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/i532-01_3g3rv.pdf