| IAグローバル検索 |
...ions with Host Devices Ethernet Connection The compact body also provides an Ethernet connector so that you can transfer read data and images via Ethernet. Smoothly transfer data to PLCs, com...
https://www.fa.omron.co.jp/data_pdf/cat/fq-cr_q186-e1_14_3_csm1000599.pdf
...l of each SSR works as a heat sink. The SSR casing serves to dissipate heat. Install the Relays so that they are adequately ventilated. If poor ventilation is unavoidable, reduce the load cur...
https://www.fa.omron.co.jp/data_pdf/cat/g3f_g3fd_ds_e_6_3_csm153.pdf
...l of each SSR works as a heat sink. The SSR casing serves to dissipate heat. Install the Relays so that they are adequately ventilated. If poor ventilation is unavoidable, reduce the load cur...
https://www.fa.omron.co.jp/data_pdf/cat/g3h_g3hd_ds_e_8_3_csm154.pdf
...tively and then tighten them evenly to 2.5 to 4.0 N·m. The silicon grease should be thin enough so that it does squirt out from between the contact surfaces when the screws are tightened. (7)...
https://www.fa.omron.co.jp/data_pdf/cat/g3ph_j177-e1_2_2_csm1000554.pdf
... prevent malfunction. Transport Do not transport the G3PJ under the following conditions. Doing so may result in damage, malfunction, or deterioration of performance characteristics. • Condit...
https://www.fa.omron.co.jp/data_pdf/cat/g3pj_j210-e1_4_3_csm1050153.pdf
... Characteristics and Reinforced Insulation for Safety Standard Compliance UL-listed components, so you can reduce the time required for the UL application process. • Using new components or u...
https://www.fa.omron.co.jp/data_pdf/cat/g3pj_j211-e1_3_1_csm1050132.pdf
...ection of the socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Otherwise, short bars may inter...
https://www.fa.omron.co.jp/data_pdf/cat/g3r-i_o_ds_e_5_11_csm2416.pdf
...ection of the socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Otherwise, short bars may inter...
https://www.fa.omron.co.jp/data_pdf/cat/g3rz_ds_e_5_2_csm2422.pdf
...ch set between two settings. Communications Unit Number Set a communications unit number on SW1 so that the host system can identify the Controller. SW1 0 1 2 3 4 5 6 7 8 9 A B C D E F Unit N...
https://www.fa.omron.co.jp/data_pdf/cat/g3za_ds_e_6_4_csm192.pdf
...e Use Transport • Do not transport the I/O Relay Terminal under the following locations. Doing so may occasionally result in damage, malfunction, or deterioration of performance characterist...
... now be connected with a short bar in the G70D-SOC08. • No tools are required to remove Relays, so Relay replacement is easier than ever. • The attached terminal cover prevents shocks. • Equi...
https://www.fa.omron.co.jp/data_pdf/cat/g70d-soc08_ds_e_5_1_csm1046356.pdf
...atches on the expansion terminal block into the mounting holes in the terminal block, and slide so that the block will not come off. • Tighten the mounting screw to fasten. (2) Attachment Ter...
https://www.fa.omron.co.jp/data_pdf/cat/g70d-vsoc16_-vfom16_ds_e_3_1_csm1046358.pdf
...e Transportation • Do not transport the I/O Relay Terminal under the following locations. Doing so may occasionally result in damage, malfunction, or deterioration of performance characterist...
https://www.fa.omron.co.jp/data_pdf/cat/g70v_j215-e1_2_20_csm1050154.pdf
...ts of 6 A or more when using this product in combination with the P7S-14F/14P/14A Socket. Doing so may result in fire. Use this product in combination with the P7S-14F-END/14P-E. Precautions ...
https://www.fa.omron.co.jp/data_pdf/cat/g7s-_-e_ds_e_7_3_csm1272.pdf
... • Do not bend a wire past its natural bending radius or pull on it with excessive force. Doing so may cause the wire disconnection. • Do not insert more than one wire into each terminal inse...
https://www.fa.omron.co.jp/data_pdf/cat/g7sa_j120-e1_12_14_csm1269.pdf
...for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, so A1 should be connected to the positive side and A2 to the negative side. Power supply input ...
https://www.fa.omron.co.jp/data_pdf/cat/g9sa-p_f106-e1_6_2_csm1070131.pdf
...for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, so A1 should be connected to the positive side and A2 to the negative side. Safety input 1 T11,...
https://www.fa.omron.co.jp/data_pdf/cat/g9sa_ds_e_11_15_csm1281.pdf
...for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, so A1 should be connected to the positive side and A2 to the negative side. Safety input 1 *1 T...
https://www.fa.omron.co.jp/data_pdf/cat/g9sb_ds_e_6_7_csm1282.pdf
...1 PLC etc. Motor controller 13 23 37 47 Note: The lock release enable signal must be configured so that it should turn ON after dangerous movement is stopped and safety is ensured for the doo...
https://www.fa.omron.co.jp/data_pdf/cat/g9se_j198-e1_4_7_csm1040781.pdf
...ures are added to your set-up. Three different models are available, with a range of I/O lines, so you can choose the most suitable for your system. Each one is compatible with the Omron conf...
https://www.fa.omron.co.jp/data_pdf/cat/g9sp_f090-e1_12_9_csm2603.pdf