| IAグローバル検索 |
...Display Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output so that the output can be switched according to the application simply by changing the wiring. ...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sx97_ds_e_1_4_csm2587.pdf
... be less than 10 m. z Installation The photomicrosensor is built into the device being used and so is not equipped to deal with interference from an external light source. When using the sens...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sy671_672_ds_e_6_4_csm486.pdf
...he output status is displayed (outputs 1, 2, 3, and 4). Note: Normally keep this pin set to OFF so that the operation status can be checked. ON: G3ZA Multi-channel Power Controller in operati...
https://www.fa.omron.co.jp/data_pdf/cat/ej1_ds_e_12_5_csm222.pdf
...he output status is displayed (outputs 1, 2, 3, and 4). Note: Normally keep this pin set to OFF so that the operation status can be checked. 7 ON: G3ZA Multi-channel Power Controller in opera...
https://www.fa.omron.co.jp/data_pdf/cat/ej1_h236-e1_4_1_csm1121137.pdf
... automatically across the entire fleet. Enterprise Manager can connect to your MES, ERP and WMS so that jobs can be propagated automatically to the fleet in real time. JOBS JOB 1 JOB 1 JOB 2 ...
https://www.fa.omron.co.jp/data_pdf/cat/enterprisemanager_i834-e-01.pdf
...hile the button on the back is pressed when power is ON. Adjust the position and mounting angle so that the laser pointer beam hits a point 15 mm above the center of the object. (The laser po...
https://www.fa.omron.co.jp/data_pdf/cat/es1-n_h227-e1_4_4_csm1059198.pdf
...the warm-up time as three seconds or more. 6. Ensure sufficient space around the main unit case so that the air vent is not covered. 7. Wire the terminals correctly after confirming the signa...
https://www.fa.omron.co.jp/data_pdf/cat/es2-hb-n_es2-thb-n_h230-e1_3_1_csm1062563.pdf
... moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do so may result in insufficient adhesion, and the Sticker may peel away from the surface. 2. When...
https://www.fa.omron.co.jp/data_pdf/cat/f03-15_ds_e_2_2_csm527.pdf
... moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do so may result in insufficient adhesion, and the Sticker may peel away from the surface. 2. When...
https://www.fa.omron.co.jp/data_pdf/cat/f03-16pe_ds_e_1_9_csm525.pdf
...3K-@@-D(Black) 2. Do not connect the Conversion Cable for the following purposes. Failure to do so may result in failure. 1. Connecting with the F39-SGIT-IL3, F39-GCNY2, F39-GCNY3 or F39-GCN5...
https://www.fa.omron.co.jp/data_pdf/cat/f3sg-sr_pg_f117-e1_1_9_csm1120108.pdf
...Bracket ) F39-LSGF ・Two b r a c ke t s p e r s e t Suitable for mounting on an aluminum profile so that its center is aligned with the center of beams. Brackets that allow beam adjustment af...
https://www.fa.omron.co.jp/data_pdf/cat/f3sg-sr_pg_f118-e1_1_6_csm1120109.pdf
...sized brackets when performing side mounting 2 for an emitter, with standard mounting brackets, so 2 for a receiver, that total of 4 per set they do not protrude from the detection surface. F...
https://www.fa.omron.co.jp/data_pdf/cat/f3sj_f074-e1_27_11_csm1816.pdf
...ious injury may possibly occur due to loss of required safety functions. Wire F3SP-B1P properly so that supply voltages or voltages for loads do NOT touch the safety inputs accidentally or un...
https://www.fa.omron.co.jp/data_pdf/cat/f3sp-b1p_ds_e_5_1_csm1067236.pdf
...sh simultaneously.) OFF ON Elevator-like lighting (Two adjacent indicators simultaneously light so that lighting moves up and down.) ON ON Accordion-like lighting (Some or all indicators simu...
https://www.fa.omron.co.jp/data_pdf/cat/f3w-d_ds_e_3_5_csm1365.pdf
...etect parts inside the bin. To detect these parts, an operator must reposition items in the bin so that the parts are within the field of view. Cameras installed at the robot arms can reduce ...
https://www.fa.omron.co.jp/data_pdf/cat/fh-smd_q298-e1_5_4_csm1108528.pdf
...ssary for developing AI detection performance. The system selects the best images for learning, so anyone can build the optimal AI model—no expert knowledge required. This dramatically saves ...
https://www.fa.omron.co.jp/data_pdf/cat/fh_q197-e1_29_1_csm1013479.pdf
...eo How-to Video Presence/Product Detection/Product type Defect Check The AI Detection Camera is so intuitive that even first-time users can set it up. Just follow the on-screen steps and conf...
https://www.fa.omron.co.jp/data_pdf/cat/fhv7-ai_q366-e1_3_1_csm1132672.pdf
...e same production line. The illuminating colors and lens focuses can be adjusted by parameters, so the mechanism for replacing lights and moving cameras is no longer necessary. This feature g...
https://www.fa.omron.co.jp/data_pdf/cat/fhv7_q264-e1_8_2_csm1066920.pdf
... screws, to prevent problems The light cover and optical filter are easy to remove and replace, so you don’t caused by the screws falling into the production line, etc. need a protective cove...
https://www.fa.omron.co.jp/data_pdf/cat/fhv7_q265-e1_9_2_csm1066921.pdf
... easily. It allow you to edit the program on the controller and the compiling is not necessary. So you can develop and adjust the system quickly. ・Microsoft® Visual Studio® and Windows are ei...
https://www.fa.omron.co.jp/data_pdf/cat/fj_q185-e1_4_5_csm1000540.pdf