| IAグローバル検索 |
...he applied voltage may fluctuate within this range. Voltages outside this range cannot be used. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...the panel or heat sink. However, by using R99-11 Mounting Brackets, the same pitch can be used. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ote:Check the manufacturer’s information for how to connect the overvoltage protection element. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...elays were mounted to the control panel. (Refer to information on mounting Solid-state Relays.) MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ote:Check the manufacturer's information for how to connect the overvoltage protection element. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...or gang mounting, if the ambient temperature is 50°C, the load current must be kept below 15 A. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
..., the inrush current from the Timer may have damaged the Sensor output. Countermeasure: Use the MY Relay or other relay to turn the Timer power supply ON/OFF. (Make sure that the contact capa...
...grammable Controllers Lead Contents FAQ No. FAQ02579 Related Contents Primary Contents Question My 8-second ON-delay timer program that uses a TIM instruction does not run properly. What is t...
...the NO contacts close before the NC contacts open. These are also called "continuous contacts." MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... contact poles? Answer It is the number of contact circuits, such as two poles or four poles. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...changeable. Note:These Relays are socket-mounted plug-in type. The Sockets are separately sold. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...N Relays model number. Specify the coil voltage after the model number as shown in the example. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...table depending on an applied load. Surge protection suitable for the applied load is required. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...DC Maximum switching current 5 A Contact form DPDT Contact structure Single Contact material Ag MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...s, refer to the following table. Be careful not to apply other voltages than the rated voltage. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...0 -6 /operation means that 1/10,000,000 failures can be expected at a reliability level of 60%. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...0 Relay Approx. 2 to 3 Capacitor Approx. 20 to 50 Resistive load 1 DC Loads and Inrush Current: MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... the NO contacts close before the NC contacts open. These are also called "continuous contacs." MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...pose Relays Socket. It cannot be connected to PCB terminals, such those on G2R-1 or G2R-2A PCB. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...et voltage I: Load (relays etc.) reset current I L : Leakage current from the Solid-state Relay MY Best-selling, general-purpose relays that can be selected based on operating environment and...