Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1461 - 14804728
faq03200

...arry current of 6 A is replaced with J7L-BR or J73L-B, the electrical durability will decrease. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq03200/

faq03402

...over 240 VAC. To operate at 400 VAC, use a transformer to reduce the voltage or use Contactors. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq03402/

faq03424

...ndurance curves can be used as indicators for the frequency of relay failures and service life. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq03424/

faq03676

...d. Comparison of Coil Surges in a 24-VDC Circuit Comparison of Coil Surges in a 200-VAC Circuit MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq03676/

faq00311

...Number of Sensors that can be connected i: Leakage current of Proximity Sensor Example: When an MY (24-VDC) Relay is used as the load, the maximum number of Sensors that can be connected is 4...

https://www.ia.omron.com/support/faq/answer/41/faq00311/

FAQ01857 for Power Controllers | OMRON Industrial ...

...ith the smallest phase angle, as shown in Fig. 2. This is how the inrush current is suppressed. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01857/

FAQ01870 for Power Controllers | OMRON Industrial ...

... time sharing SSR Good Best Good Best Pulse voltage Relay Acceptable Best Best Acceptable Relay MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01870/

FAQ01914 for Power Controllers | OMRON Industrial ...

...Xs 12 V, 40 mA (E5AN/EN, E5AK/EK) 20 12 V, 20 mA (E5CK, E5CN/GN) 20 5 V, 20 mA 20 5 V, 10 mA 20 MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01914/

FAQ01940 for Power Controllers | OMRON Industrial ...

...7.6cal/s The residual voltage means the voltage lost inside the semiconductor when it turns ON. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01940/

FAQ01955 for Power Controllers | OMRON Industrial ...

...erforms precise heater control. Some Power Regulators are called Thyristor Units and SCR Units. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01955/

FAQ01963 for Power Controllers | OMRON Industrial ...

... gradient setting is 0%, the external gradient setting can be adjusted only between 0% and 80%. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01963/

FAQ01970 for Power Controllers | OMRON Industrial ...

...ase difference may result in malfunctions. (The input signal and output amount will not match.) MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01970/

FAQ01976 for Power Controllers | OMRON Industrial ...

...(which uses a thyristor as the output element). 2. Use the G3PX-220DU (Three-phase Controller). MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01976/

FAQ01983 for Power Controllers | OMRON Industrial ...

...5% of the rated current: 4 turns Applicable models: G3PX-2[][]EC/G3PX-2[][]DC Power Controllers MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01983/

FAQ01992 for Power Controllers | OMRON Industrial ...

...ents keep in the ON state, so that oscillating waveform may occur or they may not be turned ON. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01992/

FAQ01994 for Power Controllers | OMRON Industrial ...

...7.6cal/s The residual voltage means the voltage lost inside the semiconductor when it turns ON. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01994/

FAQ01995 for Power Controllers | OMRON Industrial ...

... Protection is not provided in case of protection short circuit. Also use a quick-burning fuse. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01995/

FAQ01998 for Power Controllers | OMRON Industrial ...

...oller Note: The gradient can be changed using either the internal or external gradient setting. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq01998/

FAQ02012 for Power Controllers | OMRON Industrial ...

...etection relay output. The alarm output cannot be reset if it is wired from the secondary side. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq02012/

FAQ02022 for Power Controllers | OMRON Industrial ...

...ife can be extended. Note: Noise is generated, however, because it is not a zero-cross circuit. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/54/faq02022/

結果 1461 - 14804728

国/地域選択

Related Contents