| IAグローバル検索 |
... the load so that the load current appears to increase in order to correctly switch microloads. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ng multiple Relay coils in parallel or connecting the Relay coil in parallel with another load. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...n cause it to operate within the range of 0 V ±20 V. This voltage is called zero cross voltage. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...hat does not have a built-in surge-absorbing element (varistor) is used with an inductive load. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...s positive and negative terminals, match the polarity of Solid-state Relays when connecting it. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...into Solid-state Relays. The DC current will never become zero, therefore it will not be reset. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...produce heat by having residual voltage (voltage lost inside a semiconductor when it turns ON). MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...current required for Power MOS FET Solid-state Relays to operate normally at 200 VAC is 100 µA. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...will turn ON when the voltage is applied, thus maintaining the switching operation of the load. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... leakage current increases proportionally with the load voltage. Refer to the following graphs. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...as well as the fact that semi-conductors are susceptible to breakdown caused by short-circuits. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...tion while current flowing causes the SSR to burn out. Perform the proper wiring and soldering. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... G3CN-D, G3FD, or G3HD. Bleeder Resistance 5 VDC 1.6 kΩ 1/4 W 12 VDC 620 Ω 1 W 24 VDC 330 Ω 5 W MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... A max. Over 40 A 3.7 kW max. Over 3.7 kW Triac OK OK OK Not as good Two thyristors OK OK OK OK MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...e, the leakage current will increase, so check that the reset failure in item 1 does not occur. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... to the difference between the SSRs in operating time and reset time when the load is switched. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ns with small signal currents. G3VM Solid-state Relay is available from OMRON with NC contacts. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...to the LOAD or to the INPUT terminal? Answer The load must be connected to the LOAD terminal. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...210B Solid-state Relays, the following heating value will be obtained. P = 1.6 V x 8 A = 12.8 W MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...eep the Solid-state Relay ON. Bleeder Resistance 100 VAC 5 to 10 kΩ 3 W 200 VAC 5 to 10 kΩ 15 W MY Best-selling, general-purpose relays that can be selected based on operating environment and...