Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1421 - 14404728
faq02780

...umber have finger protection. Round crimp terminals cannot be used. Use forked crimp terminals. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02780/

faq02782

...ching Relays other than those in MY2K Series such as G2AK, MKK, and MMK General-purpose Relays. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02782/

FAQ02783 for General Purpose Relays | OMRON Indust...

...e contact point without AU plating is adopted. Contact reliability in minimum load applications MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02783/

faq02785

...2(N)-CR, MY4(N)-CR, and MY4Z(N)-CR (excluding models with special coil voltage specifications). MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02785/

faq02786

...ce life for a 220-VAC 2-A resistive load? Answer: Approximately 400,000 operations (blue line). MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02786/

FAQ02787 for General Purpose Relays | OMRON Indust...

..., the contact form, and the maximum contact current (given for a resistive load) in this table. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02787/

faq02788

...th a LY1, connect between sockets terminals 1 and 2, 3 and 4, and 5 and 6 when using over 10 A. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02788/

faq02789

...e maximum voltage that can be applied to Relays coil; it is not the continuous allowable value. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02789/

faq02790

...AC," the coil has 4 ratings, i.e., it also has "110 VAC at 50 Hz" in addition to the above. The MY and LY General-purpose Relays are examples of Relays with 4 ratings. MY Best-sellin...

https://www.ia.omron.com/support/faq/answer/36/faq02790/

faq02791

...bs the counter electromotive force (surge) generated by the coil. The same Sockets can be used. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02791/

faq02792

...A G2A-432A (Mainly for signals) 4PDT 3 A G7J DPST-NO/DPST-NC NO contacts: 25 A NC contacts: 8 A MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02792/

faq02795

...795 Related Contents Primary Contents Question Are there restrictions on the direction that the MY General-purpose Relays can be mounted? Answer  There are no restrictions. However, it is be...

https://www.ia.omron.com/support/faq/answer/36/faq02795/

faq02797

...ose Relays? Answer  LY2N have LED indicators that turn ON when voltage is applied to the coil. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02797/

faq02798

...th be used with a 110-VAC coil voltage? Answer  Yes, they can both be used because 100/110-VAC MY Series have the following four ratings. 100 VAC at 50 Hz 100 VAC at 60 Hz 110 VAC at 50 Hz 1...

https://www.ia.omron.com/support/faq/answer/36/faq02798/

faq02799

...nts Primary Contents Question What bleeder resistance is required when operating the AC coil of MY General-purpose Relays from a distance? Answer  Refer to the following table. (Typical Valu...

https://www.ia.omron.com/support/faq/answer/36/faq02799/

FAQ02800 for General Purpose Relays | OMRON Indust...

...used to judge the General Relay's lifetime. Measures used to judge the General Relay's lifetime MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02800/

faq02801

...erioration of performance of metallic materials Deterioration of performance of resin materials MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02801/

faq02803

...nswer  Yes, the same Sockets can be used. MY2N-D2 has coil polarity, so take care when wiring. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02803/

FAQ02804 for General Purpose Relays | OMRON Indust...

...ve load, an appropriate contact protection circuit can achieve almost the same characteristics. MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02804/

faq02807

...ars. (A life of 5 years is applicable when applying the rated voltage in a normal environment.) MY Best-selling, general-purpose relays that can be selected based on operating environment and...

https://www.ia.omron.com/support/faq/answer/36/faq02807/

結果 1421 - 14404728

国/地域選択

Related Contents