Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1881 - 19004543
FAQ01001 for Rotary Encoders | OMRON Industrial Au...

...measured by the output code data. The position is memorized though the power supply is cut off. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq01001/

FAQ01004 for Rotary Encoders | OMRON Industrial Au...

... and confirm whether coupling is correctly mounted or the transmission system doesn't run idle. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq01004/

FAQ02653 for Rotary Encoders | OMRON Industrial Au...

...andards certificated name-plate that is shown under the conditions of using in class 2 circuit. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq02653/

FAQ01209 for Pressure Sensors | OMRON Industrial A...

...g this into voltage, ±5% × 1⁄1000 (%) × 4 V (FS) = ±0.2 V, so the line will deviate ±0.2 V max. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01209/

FAQ01225 for Pressure Sensors | OMRON Industrial A...

...pressure in a range from -400 to 400kPa is applied within 30 seconds, the sensor is not damaged E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01225/

FAQ01238 for Pressure Sensors | OMRON Industrial A...

...it is greater than one atmosphere, and "negative pressure" when it is less than one atmosphere. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01238/

FAQ01246 for Pressure Sensors | OMRON Industrial A...

...s equivalent to a pressure of 760 mm-Hg expressed by a height of 760 mm on a mercury barometer. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01246/

FAQ01297 for Pressure Sensors | OMRON Industrial A...

...between pressure and output voltage? Answer  The relationship is given in the following graph. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01297/

FAQ01299 for Pressure Sensors | OMRON Industrial A...

...s. The Pressure Sensor "E8AA Series" can measure it. However, the flow rate cannot be measured. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01299/

FAQ01316 for Pressure Sensors | OMRON Industrial A...

... complete absence of air or any objects. It is a condition in which pressure is infinitely low. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01316/

FAQ01327 for Pressure Sensors | OMRON Industrial A...

...cm 2 ). How many Pa is 10 kgf/cm 2 ? 1 kgf/cm 2 = 0.0980665 Mpa, so 10 kgf/cm 2 = 0.980665 Mpa. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01327/

FAQ01340 for Pressure Sensors | OMRON Industrial A...

...ed, measurement errors and response delays are eliminated, which improves measurement accuracy. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01340/

FAQ01342 for Pressure Sensors | OMRON Industrial A...

...le panel and therefore the pressures for four sensors can be controlled from a single location. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01342/

FAQ01347 for Pressure Sensors | OMRON Industrial A...

...etting range. In that case, an error message will be displayed for 1 s if teaching is executed. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01347/

FAQ01350 for Pressure Sensors | OMRON Industrial A...

...ange is exceeded. For example, the Withstand pressure for E8F2-A01C Pressure Sensor is 400 kPa. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01350/

FAQ01443 for Pressure Sensors | OMRON Industrial A...

...oint is 80 kPa, and the OFF is 50 kPa, the hysteresis = 30% according to the following formula. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01443/

FAQ01447 for Pressure Sensors | OMRON Industrial A...

...E8M-10 Pressure Sensor is ±1% F.S. Converted to voltage, ±1% × 1⁄100 (%) × 4 V (F.S.) = ±0.04 V E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq01447/

faq03426

...to 2.00 kPa or 5.00 kPa whether above or below 1 kPa. Indication is not given in units of 1 Pa. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...

https://www.ia.omron.com/support/faq/answer/35/faq03426/

faq00197

...n they are mounted facing each other or in parallel. Model Item M8 M12 M18 M30 DC 2-Wire Models E2E-X[]D[] AC/DC 2-Wire Models E2E-X[]T1 Shielded A 20 30 (20) 50 (30) 100 (50) B 15 2...

https://www.ia.omron.com/support/faq/answer/41/faq00197/

FAQ00201 for Proximity Sensors | OMRON Industrial ...

... the sensing object is far and the oscillation level is high when there is a surrounding metal. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What kind of consid...

https://www.ia.omron.com/support/faq/answer/41/faq00201/

結果 1881 - 19004543

国/地域選択

Related Contents