Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1941 - 19604543
FAQ00364 for Photoelectric Sensors | OMRON Industr...

...) (*1.)E3S-GS, E3S-VS, E3L, E3S-R[]E[]series (Refer to the applicable date sheets for details.) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00364/

FAQ00379 for Photoelectric Sensors | OMRON Industr...

...rcuited with power supplies in some factors. (3) The following is output circuit diagram of the E2E as typical. E2E Standard Sensors for Detecting Ferrous Metals under Standard Condi...

https://www.ia.omron.com/support/faq/answer/43/faq00379/

faq00381

...e, temperature, sensing distance, sensing object, and angle of the sensing object are the same. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00381/

FAQ00389 for Photoelectric Sensors | OMRON Industr...

...lows to output. Please use the serial connection by the combination with the sensor controller. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00389/

faq00390

...ht from being received horizontally. This makes it possible to detect even mirror-like objects. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00390/

faq00400

...troreflective Sensors in the catalog are for measurements with the Reflector placed vertically. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00400/

faq00401

...67g protection (oil-resistant construction) is recommended for use in locations subject to oil. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00401/

faq00409

...source, further attenuation may occur if residue or dirt becomes attached to the fiber surface. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00409/

FAQ00413 for Photoelectric Sensors | OMRON Industr...

...t received are adjusted depending on a setting distance, and is set to the highest sensitivity. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00413/

FAQ00422 for Photoelectric Sensors | OMRON Industr...

...ing sensitivity volume though it depends on the customer applications and the selection models. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00422/

FAQ00428 for Photoelectric Sensors | OMRON Industr...

...x in shade. This value is changed the sunlight power. So, the value is just for your reference. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00428/

FAQ00429 for Photoelectric Sensors | OMRON Industr...

...lection. (However, the width of detection shortens by the amount of light reflection decrease.) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00429/

FAQ00438 for Photoelectric Sensors | OMRON Industr...

...not freeze by using a metallic type. However, the malfunctions might be caused by rain and fog. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq00438/

FAQ02653 for Photoelectric Sensors | OMRON Industr...

...andards certificated name-plate that is shown under the conditions of using in class 2 circuit. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02653/

faq02660

...lectors with anti-fog coating can withstand temperature changes from -25°C to room temperature. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02660/

faq02669

...: For a standard cable, a minimum bending radius of three times cables diameter is recommended. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02669/

faq02678

...sing distance for E3Z-R Photoelectric Sensors are 3 m with the E39-R1 and 4 m with the E39-R1S. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02678/

faq02947

...e:If Through-beam Sensors don’t have a sensitivity adjuster, use a slit to attenuate the light. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02947/

faq02949

...ome tilted, and the sensing distance will be extremely short. Do not use them at the same time. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq02949/

faq03100

...dirt with a dry cloth or use water. The same applies to the Sensor case if the case is plastic. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Can a Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq03100/

結果 1941 - 19604543

国/地域選択

Related Contents