Primary Contents
Machine Automation Controllers FAQ
-
Is the Power Supply Unit that is used on the CPU Rack and Expansion Rack for the NJ Series specifically for the NJ Series? Can I use the Power Supply Unit for the CJ Series instead?
-
On an NJ-series Controller, I used a variable with a TIME data type to register the timer set value for a TON instruction and other timer instructions. I want to change the set value from an NS-series Programmable Terminal, but it does not support variables with a TIME data type. How should I set the timer?
-
Can I connect an NJ-series Controller to an NSJ-series Controller via Ethernet or a serial port?
-
If I want to run an NJ-series Controller without a battery, can I disable detection of the Low Battery Error, like I can in the Programmable Controller system settings for the CS Series and CJ Series?
-
I added a Servo Drive to the EtherCAT node address network configuration in the Sysmac Studio. Then, in the I/O Map, I assigned drive variables to the I/O ports. When I added an axis setting and assigned a target node, the assignments in the I/O Map were grayed out. What should I do to access the Servo Drive?
-
According to the manual, the NJ501-1300 has a program capacity of 20 MB. How many K steps is 20 MB?
-
The performance specifications for the NJ Series lists variable tables as part of the program capacity. Why are variable tables not included in the memory capacity for variables?
-
If I need 30 licenses for the Sysmac Studio, does that mean I need to purchase 30 DVDs?
-
In the Sysmac Studio, what is the difference between Save As and Export, and Open Project and Import?
-
While creating a program, the Sysmac Studio displays a duplicate name error. What causes this error?
-
I have the CX-One. Can I use this as the Support Software for the NJ Series?
-
If I want to use data tracing for internal variables, how do I enter them in the Sysmac Studio?
-
This question is about disconnecting and connecting EtherCAT slaves. If I execute the function to disconnect a slave, is it just the specified slave that is disconnected? Do the other slaves continue to operate without stopping?
-
With the NJ Series, if I use the FileWriteVar instruction to write to a file on the SD Memory Card, can I create a CSV (comma-separated value) file if I specify the .csv extension for the filename?
-
What is the maximum number of variables that can be monitored with a data trace in the Sysmac Studio?
-
Is there a table of instruction execution times for the NJ Series?
-
On an NJ-series Controller, if I use the FilePuts instruction to write to a file on the SD Memory Card, what happens if the specified file (FileID) does not exist?
-
There are two ways to register as a user for the Sysmac Studio: by mailing the user registration post card or by using online registration. Should I use both?
-
Is there a limit to the number of user-defined function blocks and user-defined functions that I can create in an NJ-series Controller?
-
How can I protect the contacts with a surge killer?