Question
In the Sysmac Studio, what is the difference between Save As and Export, and Open Project and Import?
Answer
The Save As and Open Project commands are used with project files on your computer. The Export and Import commands are used to handle project files on another computer.
 On an NJ-series Controller, I used a variable with a TIME data type to register the timer set value for a TON instruction and other timer instructions. I want to change the set value from an NS-series Programmable Terminal, but it does not support variables with a TIME data type. How should I set the timer?
On an NJ-series Controller, I used a variable with a TIME data type to register the timer set value for a TON instruction and other timer instructions. I want to change the set value from an NS-series Programmable Terminal, but it does not support variables with a TIME data type. How should I set the timer?
                 Is there a limit to the number of user-defined function blocks and user-defined functions that I can create in an NJ-series Controller?
Is there a limit to the number of user-defined function blocks and user-defined functions that I can create in an NJ-series Controller?
                 There are two ways to register as a user for the Sysmac Studio: by mailing the user registration post card or by using online registration. Should I use both?
There are two ways to register as a user for the Sysmac Studio: by mailing the user registration post card or by using online registration. Should I use both?