Question
What is the maximum number of variables that can be monitored with a data trace in the Sysmac Studio?
Answer
The maximum number of variables for data tracing depends on the model of the CPU Unit. In the catalog, this is listed under the specifications for maximum number of records or maximum number of points. The maximum number of sampled variables is 192 for the NJ501, and 48 for the NJ301. For both models, the maximum number of records in 10,000.
 On an NJ-series Controller, I used a variable with a TIME data type to register the timer set value for a TON instruction and other timer instructions. I want to change the set value from an NS-series Programmable Terminal, but it does not support variables with a TIME data type. How should I set the timer?
On an NJ-series Controller, I used a variable with a TIME data type to register the timer set value for a TON instruction and other timer instructions. I want to change the set value from an NS-series Programmable Terminal, but it does not support variables with a TIME data type. How should I set the timer?
                 Is there a limit to the number of user-defined function blocks and user-defined functions that I can create in an NJ-series Controller?
Is there a limit to the number of user-defined function blocks and user-defined functions that I can create in an NJ-series Controller?
                 There are two ways to register as a user for the Sysmac Studio: by mailing the user registration post card or by using online registration. Should I use both?
There are two ways to register as a user for the Sysmac Studio: by mailing the user registration post card or by using online registration. Should I use both?