Page top

Lead Contents

FAQ03605 of RFID Systems FAQ

FAQ No. FAQ03605

Primary Contents


What is the width of narrow bars that can be read using the V520-R221 Bar Code Readers with a reading range of 27.5 to 52.5 mm?


The catalog and manual of the V520-R221 specify the reading range as JAN1.0.

The JAN1.0 narrow bar width is 0.33 mm.

Recommended Products


Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Port.


Cost-effective CP1E with Enhanced Expandability for Analog and Temperature Control


Motion, Logic, Safety, Vision and HMI in one

Other RFID Systems FAQ