By converting analog sensor signals to IO-Link, process data can be transmitted as digital signals, reducing the cost required for wiring from the control panel to the equipment. Increases flexibility in equipment design and facility layout.
IO-Link AD Converter
last update: November 4, 2025
By converting analog sensor signals to IO-Link, process data can be transmitted as digital signals, reducing the cost required for wiring from the control panel to the equipment. Increases flexibility in equipment design and facility layout.
Until now, when connecting a controller inside a control panel to an analog sensor on the equipment side, it was necessary to run more cables than the number of sensors. By connecting the K3CV to an IO-Link master unit, the amount of wiring between the control panel and the equipment can be reduced.
1/8 turn SmartClick for easy connection without tools.
Highly visible LED display indicates operating status/errors. Nameplates simplify equipment management.
last update: November 4, 2025