| Functions |
Description |
Cycle Time
Management |
Minimum Cycle Time |
A minimum cycle time can be set.
(0.2 to 32,000 ms; Unit: 0.1 ms)
The minimum cycle time setting can be changed
in MONITOR mode |
| Cycle Time Monitoring |
The cycle time is monitored.
(10 to 40,000 ms; Unit: 10 ms) |
| Background Processing |
Instructions with long execution times can be
executed over multiple cycles to prevent fluctuations
in the cycle time. |
Unit (I/O)
Management |
Basic I/O
Units,
Special I/O
Units, and
CPU Bus
Units |
I/O
Refreshing |
Cyclic
Refreshing |
Cyclic refreshing of Basic I/O Units, Special I/O Units,
and CPU Bus Units |
Immediate
Refreshing |
I/O refreshing by immediate refreshing instructions |
Refreshing
by IORF |
I/O refreshing by IORF instruction |
Unit Recognition at
Startup |
The number of units recognized when the power is
turned ON is displayed. |
Basic I/O
Units |
Input Response Time
Setting |
The input response times can be set for Basic I/O
Units.
The response time can be increased to reduce the
effects of chattering and noise at input contacts.
The response time can be decreased to enable
detecting shorter input pulses. |
| Load OFF Function |
All of the outputs on Basic I/O Units can be turned
OFF when an error occurs in RUN or MONITOR
mode. |
Basic I/O Unit Status
Monitoring |
Alarm information can be read from Basic I/O Units
and the number of Units recognized can be read. |
Special I/O
Units and
CPU Bus
Units |
Reading/writing data
using instructions for
specific Units |
Special instructions can be used to read/write
required data for specific Units at high speed. |
Unit Restart Bits to
Restart Units |
A Special I/O Unit or CPU Bus Unit can be
restarted. |
Configuration
Management |
Automatic I/O Allocation
at Startup |
I/O words can be automatically allocated to the
Basic I/O Units that are connected in the PLC to
start operation automatically without registering
Units into I/O tables. |
| I/O Table Creation |
The current unit configuration can be registered in
I/O tables to prevent it from being changed, to
reserve words, and to set words. |
Rack/Slot First Word
Settings |
The first words allocated to a Units on the Racks
can be set. |
Pulse I/O
Functions
(When
using
Pulse I/O
Module) |
Pulse Input
Functions |
Normal Inputs |
Input signals are read during I/O refreshing and
stored in I/O memory. |
| Interrupt Inputs |
An interrupt task can be started when an input
signal turns ON or turns OFF. |
| Quick-response Inputs |
Input signals that are shorter than the cycle time
are read and stored in I/O memory. |
High-speed Counter
Inputs |
High-speed pulse signals are counted. Interrupt
tasks can also be started. |
Pulse Output
Functions |
Normal Outputs |
The status of I/O memory is output during I/O
refreshing. |
| Pulse Outputs |
A pulse signal is output with the specified
frequency and number of pulses at a fixed duty
ratio (50%). |
| PWM Outputs |
A pulse signal is output at the specified duty ratio. |
| Origin Searches |
The origin point of the machine is determined
according to the specified origin search
parameters while actually outputting pulses and
using the origin and origin proximity input signals
as conditions.
(Pulse inputs and outputs are also used for this
function.) |
Memory
Management |
Holding I/O Memory when
Changing Operating Modes |
The status of I/O memory can be held when the
operating mode is changed or power is turned ON.
The forced-set/reset status can be held when the
operating mode is changed or power is turned ON. |
| File Memory |
Files (such as program files, data files, and
symbol table files) can be stored in Memory Card,
EM File Memory, or Comment Memory. |
| Built-in Flash Memory |
The user program and Parameter Area can be
backed up to an internal flash memory when
they are transferred to the CPU Unit. |
| EM File Function |
Parts of the EM Area can be treated as file memory. |
| Storing Comments |
I/O comments can be stored as symbol table files
in a Memory Card, EM file memory, or comment
memory. |
| EM Configuration |
EM Area can be set as trace memory or EM file memory. |
Battery-free I/O Memory
Backup Function |
This function holds DM Area (D), EM Area (E),
Holding Area (H), Counter (C), and Auxiliary
Area (A) data without the need for a battery when
the power is interrupted. |
| Memory Cards |
Automatic File Transfer at Startup |
A program file and parameter files can be read
from a Memory Card when the power is turned
ON. |
Program Replacement during
PLC Operation |
User programs can be transferred from a Memory
Card to CPU Unit during operation. |
Function for Reading and
Writing Data from a
Memory Card |
Data in I/O memory in the CPU Unit can be written
to a Memory Card in CSV/TXT format. Data in
CSV/TXT format in the Memory Card can be read to
I/O memory in the CPU Unit. |
| Communications |
--- |
|
Peripheral (USB) Port |
Bus for communications with various kinds of
Support Software running on a personal
computer. |
| Serial Port |
--- |
|
Host Link (SYSWAY)
Communications |
Host Link commands or FINS commands placed
between Host Link headers and terminators can
be sent from a host computer or PT to read/write
I/O memory, read/control the operating mode, and
perform other operations for PLC. |
No-protocol
Communications |
I/O instructions for communications ports (such
as TXD/RXD instructions) can be used for data
transfer with peripheral devices such as bar
code readers and printers. |
NT Link
Communications |
I/O memory in the PLC can be allocated and
directly linked to various PT functions, including
status control areas, status notification areas,
touch switches, lamps, memory tables, and
other objects. |
| Peripheral Bus |
Bus for communications with various kinds of
Support Software running on a personal
computer. |
| Serial Gateway |
This gateway enables receiving and automatically converting FINS to the CompoWay/F. |
| Serial PLC Links |
Data is exchanged between CPU Units using
serial ports without communications
programming. PTs set to the 1:N NT Link
protocol can be included in the network. |
| EtherNet/IP Port *1 |
100Base-TX/10Base-T
Protocols: TCP/IP, UDP, ARP, ICMP (ping only),
BOOTP, LLDP
Applications: FINS, CIP, SNTP,
DNS (Client), FTP (Server), Modbus (Server) |
|
CIP
Commu-
nications
Service |
Tag Data
Links |
Programless cyclic data exchanges with the
devices on the EtherNet/IP network. |
Message
Commu-
nications |
Any CIP commands can be received from the
devices on the EtherNet/IP network. |
FINS
Commu-
nications
Service |
Message
Commu-
nications |
Any FINS commands can be transferred with the
devices on the EtherNet/IP network. |
Socket
service |
Message
Commu-
nications |
Any data can be sent and received to and from
general-purpose devices over Ethernet. |
Modbus
Commu-
nications
Service |
Message
Commu-
nications |
Modbus commands can be sent and received to
and from Modbus clients and Modbus servers
on an EtherNet/IP network. |
| Interrupt |
Scheduled Interrupts |
A task is executed at a specified interval. |
|
Resetting and
restarting with MSKS |
When MSKS is executed, the internal timer is
restarted and the time to first interrupt is set to a
fixed value. |
Reading present value
of internal timer with
MSKR |
MSKR can be used to read the time that has
elapsed until the scheduled interrupt is started or
since the previous scheduled interrupt. |
| Power OFF Interrupts |
A task can be executed when CPU Unit's power
turns OFF. |
| I/O Interrupts |
A task can be executed when an input signal is
input to an Interrupt Input Unit. |
| External Interrupts |
A task can be executed when interrupts are
requested from a Special I/O Unit or a CPU Bus
Unit. |
Input Interrupt Function of Pulse
I/O Module |
A task is started for an interrupt input from a Pulse
I/O Module or for a high-speed counter input. |
|
Input Interrupts |
Interrupt tasks are executed when the interrupt
input turns ON or turns OFF.
Direct Mode: An interrupt task is executed each time
an input signal changes.
Counter Mode: Changes in the input signal are
counted up or down and the interrupt task is
executed when the counter counts out.
(The maximum response frequency is 3 kHz.) |
High-speed Counter
Interrupts |
An interrupt task is executed when preset
comparison conditions for a high-speed counter
are met.
Target-value comparison:
The interrupt task is executed when the count
matches a specified value.
Range comparison:
The interrupt task is executed when the count enters
or leaves a specified range of values. |
| Clock |
Clock Function |
Clock data is stored in memory.
Accuracy (Accuracy depends on the temperature.)
Ambient temperature of 55°C: -3.5 to 0.5 min error
per month
Ambient temperature of 25°C: -1.5 to 1.5 min error
per month
Ambient temperature of 0°C: -3 to 1 min error
per month |
| Built-in Capacitor Backup Time |
At ambient temperature of 40°C: 10 days |
| Operation Start Time Storage |
The time when operating mode was last changed
to RUN mode or MONITOR mode is stored. |
| Operation Stop Time Storage |
The last time a fatal error occurred or the last time
the operating mode was changed to PROGRAM
mode is stored. |
| Startup Time Storage |
The time when the power was turned ON is stored. |
| Power Interruption Time Storage |
The time when the power is turned OFF is stored. |
| Total Power ON Time Calculation |
The total time that the PLC has been ON is stored
in increments of 10 hours. |
| Power ON Clock Data Storage |
A history of the times when the power was turned
ON is stored. |
User Program Overwritten Time
Storage |
The time that the user program was last overwritten
is stored. |
| Parameter Date Storage |
The time when the Parameter Area was overwritten
is stored. |
| Power Supply Management |
Memory Protection |
Holding Area data, DM Area data, EM Area data,
Counter Completion Flags, and counter present
values are held even when power is turned OFF.
CIO Area, Work Area, some Auxiliary Area data, and
Timer Completion Flags, timer present values,
index registers, and data registers can be protected
by turning ON the IOM Hold Bit in the Auxiliary Area,
and by also setting the IOM Hold Bit to “Hold” in
the PLC Setup. |
| Power OFF Detection Time Setting |
The detection time for power interruptions can be
set.
AC power supply: 10 to 25 ms (variable)
DC power supply: 2 to 5 ms (CJ1W-PD022) or 2
to 20 ms (CJ1W-PD025) |
| Power OFF Detection Delay Time |
The detection of power interruptions can be
delayed: 0 to 10 ms (Not supported by the
CJ1W-PD022.) |
Number of Power Interruptions
Counter |
The number of times power has been interrupted
is counted. |
| Function Blocks |
Standard programming can be encapsulated as
function blocks. |
|
Languages in Function Block
Definitions |
Ladder programming or structured text |
| Debugging |
Online Editing |
The program can be changed during operation
(in MONITOR or PROGRAM mode), except for
block programming areas. |
| Force-Set/Reset |
Specified bits can be set or reset.
A parameter can be set to enable force-setting/
resetting bits in EM Area banks.
Force-setting/resetting is enabled for the specified
bank and all the banks after it. |
| Differentiate Monitoring |
ON/OFF changes in specified bits can be monitored. |
| Data Tracing |
The specified I/O memory data can be stored in the
trace memory in the CPU Unit.
The triggers can be set. |
|
Continuous Tracing |
The trace data can be uploaded during data tracing
using the CX-Programmer.
This enables continuously logging the data by
constantly uploading the trace data. |
Automatically starting
tracing when operation
starts |
Data tracing can be automatically started when
operation is started (i.e., when the operating mode
is changed from PROGRAM mode to MONITOR or
RUN mode). |
Storing Location of Error when an
Error Occurs |
The location and task number where execution
stopped for a program error is recorded. |
| Program Check |
The programs can be checked for items such as no
END instruction and FALS/FAL errors at startup. |
Self-
diagnosis
and
Restoration |
Error Log |
A function is provided to store predefined error
codes in CPU Unit, error information, and time at
which the error occurred. |
| CPU Error Detection |
CPU Unit WDT errors are detected. |
| User-defined Failure Diagnosis |
Errors can be generated for user-specified
conditions:
Non-fatal errors (FAL) and fatal errors (FALS).
Program section time diagnosis and program
section logic diagnosis are supported
(FPD instruction). |
| Load OFF Function |
This function turns OFF all outputs from Output
Units when an error occurs. |
| RUN Output |
The RUN output from the CJ1W-PA205R turns ON
while CPU Unit is in RUN mode or MONITOR mode. |
| Basic I/O Load Short-circuit Detection |
This function provides alarm information from Basic
I/O Units that have load short-circuit protection. |
| Failure Point Detection |
The time and logic of an instruction block can be
analyzes using the FPD instruction. |
| CPU Standby Detection |
This function indicates when the CPU Unit is on
standby because all Special I/O Units and CPU Bus
Units have not been recognized at the startup in
RUN or MONITOR mode. |
Non-fatal Error
Detection |
System FAL Error
Detection (User-
defined non-fatal error) |
This function generates a non-fatal (FAL) error when
the user-defined conditions are met in program. |
Duplicated Refreshing
Error Detection |
This function detects an error when an immediate
refreshing Instruction in an interrupt task is
competing with I/O refreshing of a cyclic task. |
Basic I/O Unit Error
Detection |
This function detects the errors in Basic I/O Units. |
Backup Memory
Error Detection |
This function detects errors in the memory backup
of the user programs and parameter area (backup
memory). |
| PLC Setup Error Detection |
This function detects setting errors in the PLC Setup. |
CPU Bus Unit Error
Detection |
This function detects an error when there is an error
in data exchange between the CPU Unit and a CPU
Bus Unit. |
Special I/O Unit Error
Detection |
This function detects an error when there is an error
in data exchange between the CPU Unit and a
Special I/O Unit. |
Tag Memory Error
Detection |
This function detects errors in tag memory. |
| Battery Error Detection |
This function detects an error when a battery is not
connected to the CPU Unit or when the battery
voltage drops. |
CPU Bus Unit Setting
Error Detection |
This function detects an error when the model of a
CPU Bus Unit in the registered I/O tables does not
agree with the model that is actually mounted in the
PLC. |
Special I/O Unit Setting
Error Detection |
This function detects an error when the model of a
Special I/O Unit in the registered I/O tables does not
agree with the model of Unit that is actually mounted. |
Fatal
Error
Detection |
Memory Error Detection |
This function detects errors that occur in memory of
the CPU Unit. |
| I/O Bus Error Detection |
This function detects when an error occurs in data
transfers between the Units mounted in Rack slots
and the CPU Unit and detects when the End Cover
is not connected to the CPU Rack or an Expansion
Rack. |
Unit/Rack Number
Duplication Error |
This function detects an error when the same unit
number is set for two or more Units, the same word
is allocated to two or more Basic I/O Units, or the
same rack number is set for two or more Racks. |
Too Many I/O Points
Error Detection |
This function detects an error when the total number
of I/O points set in the I/O tables or the number of
Units per Rack exceeds the specified range. |
I/O Setting Error
Detection |
The registered I/O tables are used to detect errors
if the number of Units in the registered I/O tables
does not agree with the actual number of Units
that are connected or an Interrupt Unit has been
connected in the wrong position. |
| Program Error Detection |
This function detects errors in programs. |
|
Instruction
Processing
Error
Detection |
This function detects an error when the given data value is invalid when executing an instruction, or execution of instruction between tasks was attempted. |
Indirect
DM/EM
BCD Error
Detection |
This function detects an error when an indirect
DM/EM address in BCD mode is not BCD. |
Illegal Area
Access
Error
Detection |
This function detects an error when an attempt is
made to access an illegal area with an instruction
operand. |
No END
Error
Detection |
This function detects an error when there is no END
instruction at the end of the program. |
Task Error
Detection |
This function detects an error when there are no
tasks that can be executed in a cycle, there is no
program for a task, or the execution condition for an
interrupt task was met but there is no interrupt task
with the specified number. |
Differen-
tiation
Overflow
Error
Detection |
This function detects an error when too many
differentiated instructions are entered or deleted
during online editing (131,072 times or more). |
Invalid
Instruction
Error
Detection |
This function detects an error when an attempt is
made to execute an instruction that is not defined in
the system. |
User
Program
Area
Overflow
Error
Detection |
This function detects an error when instruction data
is stored after the last address in user program area. |
Cycle Time Exceeded
Error Detection |
This function monitors the cycle time (10 to
40,000 ms) and stops the operation when the set
value is exceeded. |
System FALS Error
Detection (User-
defined Fatal Error) |
This function generates a fatal (FALS) error when
the user-defined conditions are met in program. |
| Version Error Detection |
This function detects an error when a user program
includes a function that is not supported by the
current unit version. |
Memory Card Transfer
Error Detection |
This function detects an error when the automatic
file transfer from Memory Card fails at startup. |
| Maintenance |
Simple Backup Function |
This function collectively backs up the data in CPU
Unit (user programs, parameters, and I/O memory)
and internal backup data in the I/O Units. |
| Unsolicited Communications |
A function that allows the PLC to use Network
Communications Instruction to send required FINS
commands to a computer connected via a Host Link |
| Remote Programming and Monitoring |
Host Link communications can be used for remote
programming and remote monitoring through a
Controller Link, Ethernet, DeviceNet, or SYSMAC
LINK Network.
Communications across network layers can be
performed. Controller Link or Ethernet: 8 layers
DeviceNet or SYSMAC LINK: 3 layers |
Automatic Online
Connection via
Network |
Direct
Connection |
This function enables automatically connecting to
the PLC online when the CX-Programmer is directly
connected by a serial connection (peripheral (USB)
port or serial port). |
Via
Networks |
This function enables connecting the
CX-Programmer online to a PLC that is connected
via an EtherNet/IP network. |
| Security |
Read Protection using Password |
This function protects reading and displaying programs and tasks using passwords.
Write protection: Set using the DIP switch.
Read protection: Set a password using the
CX-Programmer. |
| FINS Write Protection |
This function prohibits writing by using FINS
commands sent over the network. |
| Unit Name Function |
This function allows the users to give any names to
the Units. Names are verified at online connection
to prevent wrong connection |
| Hardware ID Using Lot Numbers |
This function sets operation protection by identifying
hardware using the user programs according to lot
numbers stored in the Auxiliary Area. |
| Operation Log Function |
Function for recording important operations and the
results of operations performed by online users
while they are online together with the date, IP
address of PC, and user name. |
| Extended FINS Write Access Log |
Function for retaining a log of requests to write to
the CPU Unit from external sources when the
source address is not the local node. |
| File Encryption Function |
Function for encrypting files handled by
CX-Programmer, backup tools, and file memory to
prevent unauthorized access by third parties. |
| Secure Communications Function *2 |
Function for ensuring the confidentiality and integrity
of the line used to access important data on the
CPU Unit from peripheral tools. |
| User authentication *2 |
Function for allowing only specified users to perform
online operation from peripheral tools to further
restrict online operation based on privileges set for
each user. |
| Port Open/Close Function *2 |
Function for allowing you to block or allow
communications to pass through the TCP/ UDP
ports allocated to individual communication
functions according to the configured setting. |
| IP Packet Filter *2 |
Function for selectively allowing packets received by
the EtherNet/IP port to pass through based on
preset conditions. |