Question
What is the maximum length of a cable connected to the Laser Measurement Sensors, Smart Amplifier "ZX-L"?
Answer
For Reflective Type Sensor Head: 20.6 m (Cable length when shipped from the factory 0.6 m + extension 20 m)
For Through-beam Type Sensor Head: 10.1 m (Cable length when shipped from the factory 2.1 m + extension 8 m)
For Amplifier Unit: 20 m (Cable length when shipped from the factory 2 m + extension
Description
1. Length of a cable connected to the Sensor Head when shipped from the factory
Pull-out length of a cable connected to the Reflective Type Sensor Head when shipped from the factory is 0.5 m.
Thus, in the case of the Reflective Type Sensor, secured length of a cable between the Sensor Head and the Amplifier Unit is 0.5 m + 13.3 cm = 63 cm when shipped from the factory.
(1) Reflective sensor head
Pull-out length of a cable connected to the Through-beam Type Sensor Head when shipped from the factory is 0.5 m, and a 1.5 m-long Y-shaped bifurcated Sensor Head - Amplifier unit Connection Cable is included with shipment. Thus, in the case of the Through-beam Type Sensor Head, secured length of a cable between the Sensor Head and the Amplifier Unit is 0.5 m + 1.5 m + 13.3 cm = 2 m 13 cm when shipped from the factory.
(2) Through beam sensor head
2. When a cable connected to the Sensor Head is extended
When the above mentioned cable connected to the Sensor Head is further extended than it is shipped from the factory, be sure to use the following Extension Cable "ZX-XC Series".
Extension Cable
Optional
ZX-XC1A (Cable Length = 1 m)
ZX-XC4A (Cable Length = 4 m)
ZX-XC8A (Cable Length = 8 m)
ZX-XC8A (Cable Length = 9 m)
ZX-XC8A (Cable Length = 9 m)
Example 1:
When a cable connected to the Reflective Type Sensor Head is extended up to 20.6 m, use the following cables in combination.
Formula:
Length of a cable connected to the Sensor Head when shipped from the factory (0.5m) + 13.3 cm
+ ZX-XC9A (Cable Length = 9 m) × 2 + ZX-XC1A (Cable Length = 1 m) × 2
= 0.5 m + 13.3 cm + 18 m + 2 m
= 20.6 m
Example 2:
When a cable connected to the Through-beam Type Sensor Head is extended up to 10.1 m
Formula:
Length of a cable connected the Sensor Head when shipped from the factory (2 m)+ 13.3 cm
+ ZX-XC8A (Cable Length = 8 m) × 1
= 2 m + 13.3 cm + 8 m
= 10.1 m
3. Length of a cable connected to the Amplifier Unit when shipped from the factory
Length of a cable connected to the Amplifier Unit when shipped from the factory is as follows.
ZX-LDA11 (Cable Length = 2 m, NPN Output)
ZX-LDA11 (Cable Length = 10 m, NPN Output)
ZX-LDA41 (Cable Length = 2 m, PNP Output)
4. When a cable connected to the Amplifier Unit is extended
When the above mentioned cable connected to the Amplifier Unit is further extended than it is shipped from the factory, be sure to use the same type of shielded cables (shield specifications for the Amplifier Unit: 0.1 mm in diameter, 51 shielded wires).
Standard Sensors for Detecting Ferrous Metals under Standard Conditions