... Model Number Description E3Z-G61 0.5M Grooved type photoelectric sensor, Grooved Type, Sensing distance: 25 mm, NPN open collector, 1 axes, Pre-wired model, 0.5 m E3Z-G61 2M Grooved type pho...
...he line beam lens reduces tact time. Diffuse illumination head x diffusing lens for curing at a distance This combination maintains the irradiation power of 800 mW/cm 2 for curing even when t...
... the system that meets the requirements. Two Series of Expansion Racks Up to 50 m Long for Long-distance Expansion with Up to 72 Units and 7 Racks With an expansion capacity of up to 80 Units...
...angle (directional angle) listed in the catalog specifications is within ±2.5° when the sensing distance for the emitter and receiver is at least 3m. This means that the effective aperture an...
...sors Lead Contents FAQ No. FAQ02323 Related Contents Primary Contents Question What is a safety distance? Answer Minimum Distance from the Detection Zone to the Danger Zone The saf...
...contact work? Answer If an NO contact becomes welded, all NC contacts will maintain a minimum distance of 0.5 mm when the coil is not energized. Likewise if an NC contact becomes welded, al...
...tents FAQ No. FAQ02676 Related Contents Primary Contents Question How large is the differential distance for Photomicro Sensors? Answer The distance depends on the model, but use t...
...open collector signal to turn ON or OFF. Noise immunity can be improved by shortening the cable distance, using a shielded cable, or by using a capacitor. Line Driver The differential line dr...