...r's Measurement Head of D5V cannot be replaced. The Flat Actuator, D5V[]-3F1, has an M2.5 screw so the Measurement Head can be replaced. Models that have a replaceable Measurement Head are th...
... above 1 μm. Heat rays emitted from the hot object are similar in wavelength to the laser beam, so the receiver element may detect the heat rays. Conduct tests with the actual system to deter...
... the Operation Unit or the Socket Unit. The lever has a hole with an inside diameter of 6.5 mm, so the lever can be moved in the specified direction by inserting a screwdriver into the hole a...
...Extractor. 2.Mounting the LED The following figure shows the mounting direction. Insert the LED so that the protrusions on the LED line up with the narrow guides on the socket unit. 3.Mountin...
...m/h × (0.006%) = ±0.0051 km/h In this case, three digits are displayed below the decimal point, so the fourth digit below the decimal point in ±0.0051 km/h is rounded off to yield an accuracy...
...swer The CT has specific wiring and the Power Sensor has polarity (see Figure 1). Wire the CT so that the load side of the sensing line is on the side of the CT with the label "L" and the p...
...lays operating the instant that an overcurrent is detected. A starting current flows in motors, so Relays do not operate for a certain time during startup and then switches to instantaneous r...
...90 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the power is turned ON? Answer See the prog...
...99 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the contact turns OFF? (downward differentiat...
...04 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the contact turns ON? (upward differentiation...