Primary Contents

Site Search Results

Site Search Product Search
Results 441 - 450 of 1179
FAQ00653 for Temperature Controllers | OMRON Indus...
... over a controlled object would be difficult if heating was the only type of control available, so cooling control was also added. Two control outputs (one for heating and one for cooling) ca...

https://www.ia.omron.com/support/faq/answer/53/faq00653/

FAQ01870 for Power Controllers | OMRON Industrial ...
...ks, thereby extending the service life of the heater. 3.The gradient can be set as desired, and so the output amount can be set when a Power Controller is used in a set with a Temperature Con...

https://www.ia.omron.com/support/faq/answer/54/faq01870/

FAQ01992 for Power Controllers | OMRON Industrial ...
...t is less than 1A, decrease in output signals cannot make output elements keep in the ON state, so that oscillating waveform may occur or they may not be turned ON. MY Best-selling, general-p...

https://www.ia.omron.com/support/faq/answer/54/faq01992/

faq00502
...ween the HIGH threshold value and the LOW threshold value is smaller than the hysteresis value, so that a PASS judgment is not possible. The setting is thus not allowed. Remedy 2: Make the hy...

https://www.ia.omron.com/support/faq/answer/56/faq00502/

faq01222
...ge remains the same until the next nth sampling is taken. It is simply the average of n samples so it has nothing to do with the previous data. The output response is slower for simple averag...

https://www.ia.omron.com/support/faq/answer/56/faq01222/

faq01289
...hicle on expressway, motorcycle and etc.) 3. High-temperature objects Surrounding air is heated so that ultrasonic waves may be reflected. E2E Standard Sensors for Detecting Ferrous Metals un...

https://www.ia.omron.com/support/faq/answer/56/faq01289/

faq01307
...y the other three settings as described above. The effectiveness depends on the sensing object, so always confirm operation with the actual system. E2E Standard Sensors for Detecting Ferrous ...

https://www.ia.omron.com/support/faq/answer/56/faq01307/

faq01335
...ure compensation function makes it easy to set the measurement range. The Sensor is ultrasonic, so it is not affected by the color of objects. Perform a variety of control operations by combi...

https://www.ia.omron.com/support/faq/answer/56/faq01335/

faq01356
...fect E4PA Ultrasonic Sensor? Answer  The Ultrasonic Switch uses air as the translation medium, so it is easily affected by wind. Care must be taken when using this Sensor but the E4PA is the...

https://www.ia.omron.com/support/faq/answer/56/faq01356/

faq03137
...ll appear instead of the warming-up display. Warming up itself, however, will not be completed, so high-accuracy measurements will not be possible. Also, ZX-L-N Laser type does not have this ...

https://www.ia.omron.com/support/faq/answer/56/faq03137/

Results 441 - 450 of 1179