...S Reflectors? Answer E39-R1S has better reflection efficiency and directionality than E39-R1, so more light returns to the receiver, which enables a longer sensing distance. For reference, ...
...d how can it be corrected? Answer Retroreflective Sensors normally have the MSR function, and so shiny sensing objects can also be detected. Perform a test before using Sensors for sensing ...
.... Does voltage need to be applied to both of these? Answer No. They are internally connected, so only one of them needs to be powered. Applicable models: M7E-08,M7E-12, M7E-20, and M7F Digi...
...r of these happens, vibrations similar to earthquakes are probably being detected in that area, so change the installation location. E2E Standard Sensors for Detecting Ferrous Metals under St...
...dicator (red LED) will begin to flash. Countermeasure: Place the Sensors apart from one another so that they do not interfere with each other. E2E Standard Sensors for Detecting Ferrous Metal...
...ure compensation function makes it easy to set the measurement range. The Sensor is ultrasonic, so it is not affected by the color of objects. Perform a variety of control operations by combi...
...edium. In normal atmosphere, reflection from any object (even human bodies) is well transmitted so detection of that object is easy. E2E Standard Sensors for Detecting Ferrous Metals under St...
...re changed. (2) Correcting PID constants when there is external disturbances in the temperature so that the temperature falls within a specified range. (3) Correcting PID constants when hunti...
...h. The extension will cause the resistance of the lead wires to affect the display temperature, so use lead wires with thick conductors. (OMRON does not carry lead wires for extension. Use co...
...it set on the E5[]N? Answer 1. Direct/Reverse Operation (1) Direct operation performs control so that the manipulated variable is increased when the process value increases. Reverse operati...