Primary Contents

Site Search Results

Site Search Product Search
Results 421 - 430 of 1179
faq00348
...igures, there is no problem if the magnet section (GLS-M1) is rotated 180°. However, install it so that the direction of travel is in the direction of the arrow. The sensing distance will dec...

https://www.ia.omron.com/support/faq/answer/41/faq00348/

faq00363
...ber of Sensors used increases the probability of oscillating frequencies coming close together, so mount the Sensors at distances of at least the catalog values. E2E Standard Sensors for Dete...

https://www.ia.omron.com/support/faq/answer/41/faq00363/

faq00414
...e following characteristics: Internal electronic components are placed in the amplifier section so that they are not subjected to high temperatures. Heat-resistant parts are used for the case...

https://www.ia.omron.com/support/faq/answer/41/faq00414/

faq02657
...igure 1, the surface of the detection coil on Shielded Proximity Sensors is covered with metal, so the flux is concentrated at the front of Sensors, which reduces the influence of surrounding...

https://www.ia.omron.com/support/faq/answer/41/faq02657/

faq02666
...collector output is used, current will flow to F92A in one direction, as shown in Figure 2, and so the change in impedance input to Proximity Sensors will be reduced by half. To obtain the sa...

https://www.ia.omron.com/support/faq/answer/41/faq02666/

faq03386
...ectrostatic capacitance will also change when the status of the electrical load is changed, and so stable detection cannot be performed. For stable detection, it is recommended to first ioniz...

https://www.ia.omron.com/support/faq/answer/41/faq03386/

FAQ00227 for Photoelectric Sensors | OMRON Industr...
...se make the hole of the same size as the lens diameter basically. Please refer to the following so that the idea is different depending on the sensing method. 1. Idea to use the light through...

https://www.ia.omron.com/support/faq/answer/43/faq00227/

FAQ00320 for Photoelectric Sensors | OMRON Industr...
...dual photodiode through a light receiving lens. The position of the dual photodiode is adjusted so that N side and F side of the dual photodiode become the same amount of receiving light, and...

https://www.ia.omron.com/support/faq/answer/43/faq00320/

faq00390
...ill make it impossible to detect the object. The light will not be polarized at the object, and so the polarizing filter at the light-receiving side will prevent the reflected light from bein...

https://www.ia.omron.com/support/faq/answer/43/faq00390/

FAQ00428 for Photoelectric Sensors | OMRON Industr...
...of the illuminance is approx. 10,000 lx max in shade. This value is changed the sunlight power. So, the value is just for your reference. E2E Standard Sensors for Detecting Ferrous Metals und...

https://www.ia.omron.com/support/faq/answer/43/faq00428/

Results 421 - 430 of 1179