Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 2881 - 2900 of 23123
FAQ02445 for Safety Limit Switches | OMRON Industr...

...es. Terminals 11 and 12 in the illustration are the contacts forcibly opened. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance. OS32C Compac...

https://www.ia.omron.com/support/faq/answer/31/faq02445/

faq00765

... Contents FAQ No. FAQ00765 Related Contents Primary Contents Question Why doesn't the indicator light when I turn ON the power to 61F Floatless Level Controllers? Answer  The indicator is an...

https://www.ia.omron.com/support/faq/answer/33/faq00765/

FAQ01347 for Pressure Sensors | OMRON Industrial A...

... first point : Teaching, window mode 1.Press to enter pressure setting mode. The OUT1 indicator light and the will be displayed. 2.Select one-point teaching or two-point teaching for OUT1 or ...

https://www.ia.omron.com/support/faq/answer/35/faq01347/

FAQ01922 for Push Buttons / Indicator Lamps | OMRO...

...mps Lead Contents FAQ No. FAQ01922 Related Contents Primary Contents Question The lamp does not light up even when Illuminating Type Push Button Switches are pushed. Answer  Check the follow...

https://www.ia.omron.com/support/faq/answer/38/faq01922/

FAQ01956 for Push Buttons / Indicator Lamps | OMRO...

...illumination? Answer  LED lamp illumination uses an LED with the same shape as an incandescent light bulb. The LED can be replaced because the LED lamp and the operating section are separate...

https://www.ia.omron.com/support/faq/answer/38/faq01956/

FAQ02029 for Push Buttons / Indicator Lamps | OMRO...

...escent illumination? Answer  Incandescent illumination is a lighting method using incandescent light bulbs. The incandescent light bulb and the operation unit are separate and indep...

https://www.ia.omron.com/support/faq/answer/38/faq02029/

faq00311

...ge of Proximity Sensor V S : Power voltage It is possible, however, that the indicators may not light correctly and error pulses (of approximately 1 ms) may be generated because the rated pow...

https://www.ia.omron.com/support/faq/answer/41/faq00311/

faq00380

... that are used outdoors may not last. Reasons: Degradation of Resin Material Due to Ultraviolet Light The environmental resistance (i.e., water resistance) of Proximity Sensors may be degrade...

https://www.ia.omron.com/support/faq/answer/41/faq00380/

FAQ00227 for Photoelectric Sensors | OMRON Industr...

...ic Sensors Lead Contents FAQ No. FAQ00227 Related Contents Primary Contents Question To use the light of a Photoelectric Sensor through the hole, how large the hole should be? Answer  Please...

https://www.ia.omron.com/support/faq/answer/43/faq00227/

FAQ00297 for Photoelectric Sensors | OMRON Industr...

...nts FAQ No. FAQ00297 Related Contents Primary Contents Question Isn't there problem even if two light emitted from Photoelectric Sensor of different place intersects? Answer  There is no pro...

https://www.ia.omron.com/support/faq/answer/43/faq00297/

FAQ00307 for Photoelectric Sensors | OMRON Industr...

...ead Contents FAQ No. FAQ00307 Related Contents Primary Contents Question What is "Wavelength of light "? Answer  Light is a kind of electromagnetic wave and has various wavelengths ...

https://www.ia.omron.com/support/faq/answer/43/faq00307/

FAQ00320 for Photoelectric Sensors | OMRON Industr...

...ce-setting Photoelectric Sensor detected? Answer  PSD and the dual photodiode are used for the light receiving element and the distance to the sensing object is judged by detecting the refle...

https://www.ia.omron.com/support/faq/answer/43/faq00320/

faq00359

... Photoelectric Sensors operate? Answer  There is a stability indicator (green) and an incident light indicator (red). There are four operation patterns depending on the amount of incide...

https://www.ia.omron.com/support/faq/answer/43/faq00359/

FAQ00360 for Photoelectric Sensors | OMRON Industr...

...photoelectric sensor is the one to detect presence and the state of the object by the change in light. 1. What is a photoelectric sensor? Amount of light (luminance) is converted to ...

https://www.ia.omron.com/support/faq/answer/43/faq00360/

faq00390

...ensors? Answer  MSR is a function of Retroreflective Photoelectric Sensors to receive only the light reflected from the Retroreflector by using the characteristics of the polarizing filter b...

https://www.ia.omron.com/support/faq/answer/43/faq00390/

faq00401

...r on the lens surface. (Through-beam Sensors and Retroreflective Sensors may incorrectly detect light interruption. Diffuse-reflective Sensors may incorrectly detect light incidence,...

https://www.ia.omron.com/support/faq/answer/43/faq00401/

faq00409

...g E32-T24/D24 and E32-T14L/D14L, cannot be used even with IP67 protection because in the water, light will continue through without being reflected. E39-F1/F3 also cannot be used because the ...

https://www.ia.omron.com/support/faq/answer/43/faq00409/

FAQ00413 for Photoelectric Sensors | OMRON Industr...

...n What is adjusted in the sensitivity setting of a Photoelectric Sensor? Answer  The amount of light emitted or the amount of light received are adjusted, and the sensing distance i...

https://www.ia.omron.com/support/faq/answer/43/faq00413/

FAQ00422 for Photoelectric Sensors | OMRON Industr...

...ion in through-beam photoelectric sensors? Answer  Point of mutual interference prevention The light of other sensor do not enter own receiver. Prevention methods are as follows. 1. Setting ...

https://www.ia.omron.com/support/faq/answer/43/faq00422/

FAQ00428 for Photoelectric Sensors | OMRON Industr...

...ion What happens when direct sunlight strikes to the lens of the receiver? Answer  Even if the light of a emitter is received, the sensor is the light shielding, or even if the...

https://www.ia.omron.com/support/faq/answer/43/faq00428/

Results 2881 - 2900 of 23123

Select Country in