| Site Search | Product Search | IA Global Search |
...then a turntable or positioning robot moves the workpiece to the area where the work is done. A limit switch or other means is used to detect when the robot is in a safe position, and muting ...
...energy-saving measures. Alarm Output An alarm can be output when active power exceeds a certain limit. There are two outputs; a pulse output and an output for alarm selection. Alarms can also...
... usability of your machine by enlarging these objects in size. Dynamically changing upper/lower limit value The upper and lower limit values can be dynamically changed by setting var...
... line is running at limited speed but it is not stopped. • Machine restarts smoothly from speed limit to normal speed. Reduce changeover time ISSUE • In a coil change, the machine operator ha...
...tage to change the internal oil and water shape. * Calculated using Omron’s condition below. Limit of standard mechanical autofocus : 50,000 operations Usage condition: Focus is changed...
... level. Laser class 1 for safety Combining as strong an emission as possible within the class 1 limit with the advanced device and high-frequency circuit design technology, the sensor can per...
...re all transfer contacts. The NC contact is either on the right side or on the upper side. Time-limit operating contacts A: NO contacts B: NC contacts Time-limit resetting contacts A...
https://www.ia.omron.com/support/guide/19/further_information.html
...n be maintained. At this switching speed, however, in addition to mechanical limits, there is a limit to the speed that is effective to reduce arcing (i.e., economical speed). In particular, ...
https://www.ia.omron.com/support/guide/29/explanation_of_terms.html
...ildings and apartments but due to recent Japanese government regulations that require the lower limit to be displayed, the 61F-GP-N may be added. Elevated Tank Water tanks that are installed ...
https://www.ia.omron.com/support/guide/33/explanation_of_terms.html
...lit when the Relay Unit operates. PDF Download(7575KB) Local Navigation Switches Level Switches Limit Switches Basic Switches Push Buttons / Indicator Lamps Thumbwheel Switches FAQ Technical ...
https://www.ia.omron.com/support/guide/33/troubleshooting.html
...ric strength 75% min. of initial specified value Coil resistance 95% of initial specified lower limit to 105% of initial specified upper limit Must-operate voltage 1.2 times max. of ...
https://www.ia.omron.com/support/guide/36/troubleshooting.html
...teristics E3Z-T[]1(T[]6) Characteristics ・ Through-beam Sensors: Indicates the sensing position limit for the Receiver with the Emitter at a fixed position. ・ Retro-reflective Sensors: Indi...
https://www.ia.omron.com/support/guide/43/further_information.html
...re welded. The SSR has a short-circuit fault. The PID constants are not suitable. Restricted MV limit values are set. The controlled object is heating by itself. Why does the process value os...
https://www.ia.omron.com/support/guide/53/further_information.html
...port card Product Discontinuation FIT20-MC601 Recommended Replacement CXONE-AL01D-V4 Within the limit of the ladder program, CX-One Ver.4 is upward compatible to CV series. SFC program is onl...
https://www.fa.omron.com.cn/upload/alternative/PRDN-2011272E.pdf
...revents the servomotor from rotating outside of the operating range of the device by connecting limit inputs. When the Forward Drive Prohibit Input or Reverse Drive Prohibit Input turns OFF, ...
https://www.ia.omron.com/support/guide/14/explanation_of_terms.html
...ce for connector use. The rated current is normally specified according to the temperature rise limit of the connector contact section, connection section, etc. Rated Voltage A voltage that s...
https://www.ia.omron.com/support/guide/46/explanation_of_terms.html
.... For actual performance for short circuit current, refer to the rated breaking capacity (rated limit breaking capacity Icu and rated operating breaking capacity Icu). What is the difference ...
https://www.ia.omron.com/support/guide/753/further_information.html
...ts. The motor will not rotate if a load larger than this torque is applied to the motor. Torque Limit A function that limits the output torque of a motor. DC Braking A function that applies a...
https://www.ia.omron.com/support/guide/9/explanation_of_terms.html
...for Safety Components Related Contents Lead Contents Safety Sensors Safety Door Switches Safety Limit Switches Emergency Stop Switches Safety Swich Relays with Forcibly Guided Contacts Safety...
...ロン 第16版』 『ベスト制御機器オムロン 第16版 CD-ROM版』 『リミットスイッチ/大型マイクロスイッチ 総合カタログ2004』 『LIMIT SWITCHES G. CATALOGUE』 (2003年6月発行) (2003年7月発行) (2004...